ETHFW API Guide
|
Request params for ETHREMOTECFG_CMD_DEL_FILTER_MAC command.
This structure holds vlanId, MAC address which will be used for deleting multicast MAC address from the receive filter.
Data Fields | |
EthRemoteCfg_ReqHdr | hdr |
uint8_t | macAddr [ETHREMOTECFG_MACADDRLEN] |
uint16_t | vlanId |
EthRemoteCfg_ReqHdr EthRemoteCfg_FilterMacDelReq::hdr |
Request message common header.
uint8_t EthRemoteCfg_FilterMacDelReq::macAddr[ETHREMOTECFG_MACADDRLEN] |
Multicast MAC address to be added.
uint16_t EthRemoteCfg_FilterMacDelReq::vlanId |
VLAN id.