ETHFW API Guide
|
Request params for ETHREMOTECFG_CMD_ADD_FILTER_MAC command.
This structure holds vlanId, MAC address and Rx flowIdx details used for adding multicast MAC address to the receive filter.
Data Fields | |
EthRemoteCfg_ReqHdr | hdr |
uint8_t | macAddr [ETHREMOTECFG_MACADDRLEN] |
uint16_t | vlanId |
uint32_t | flowIdxBase |
uint32_t | flowIdxOffset |
EthRemoteCfg_ReqHdr EthRemoteCfg_FilterMacAddReq::hdr |
Request message common header.
uint8_t EthRemoteCfg_FilterMacAddReq::macAddr[ETHREMOTECFG_MACADDRLEN] |
Multicast MAC address to be added.
uint16_t EthRemoteCfg_FilterMacAddReq::vlanId |
VLAN id.
uint32_t EthRemoteCfg_FilterMacAddReq::flowIdxBase |
Rx flow index base from which the MAC_address association will be added. It's applicable only for exclusive multicast traffic.
uint32_t EthRemoteCfg_FilterMacAddReq::flowIdxOffset |
Rx flow index offset.