ETHFW API Guide
|
Ethernet device data.
The framework will return the below device data to the remote client.
Data Fields | |
EthRemoteCfg_NotifyHdr | hdr |
EthRemoteCfg_FwVerInfo | fwVer |
uint64_t | permissionFlags |
uint32_t | uartConnected |
uint32_t | uartId |
EthRemoteCfg_NotifyHdr EthRemoteCfg_DeviceData::hdr |
Notify message common header.
EthRemoteCfg_FwVerInfo EthRemoteCfg_DeviceData::fwVer |
Ethernet device Firmware version info.
uint64_t EthRemoteCfg_DeviceData::permissionFlags |
Flag indicating permission enabled for each command for the connecting client.
uint32_t EthRemoteCfg_DeviceData::uartConnected |
Flag indicating if UART is connected: 1 indicates UART connected, 0 indicates UART not connected.
uint32_t EthRemoteCfg_DeviceData::uartId |
UART ID used by firmware for log prints.