ETHFW API Guide
|
Request params for ETHREMOTECFG_CMD_ATTACH or ETHREMOTECFG_CMD_ATTACH_EXT commands.
This requests provides the virtual port for which it is requesting the core attach and recevies and handle called token which will be further used by the client to communicate with the server. Each token is unique for a given virtual port.
Data Fields | |
EthRemoteCfg_ReqHdr | hdr |
uint32_t | virtPort |
EthRemoteCfg_ReqHdr EthRemoteCfg_AttachReq::hdr |
Request message common header.
uint32_t EthRemoteCfg_AttachReq::virtPort |
Virtual port which needs core attach.