ETHFW API Guide
|
Response params for ETHREMOTECFG_CMD_ALLOC_TX command.
This response holds the information of the allocated Tx channel which is PSIL channel id for the given virtual port.
Data Fields | |
EthRemoteCfg_ResHdr | hdr |
uint32_t | txPsilDstId |
EthRemoteCfg_ResHdr EthRemoteCfg_AllocTxRes::hdr |
Response message common header.
uint32_t EthRemoteCfg_AllocTxRes::txPsilDstId |
Tx PSIL peer destination thread id which should be paired with the Tx UDMA channel.