ETHFW API Guide
EthRemoteCfg_AllocRxRes Struct Reference

Detailed Description

Response params ETHREMOTECFG_CMD_ALLOC_RX command.

This response holds the information of the allocated Rx flow which is rxFlowIdxbase and rxFlowIdxoffset for the given virtual port.

Data Fields

EthRemoteCfg_ResHdr hdr
 
uint32_t rxFlowIdxBase
 
uint32_t rxFlowIdxOffset
 
uint32_t rxPsilSrcId
 

Field Documentation

◆ hdr

EthRemoteCfg_ResHdr EthRemoteCfg_AllocRxRes::hdr

Response message common header.

◆ rxFlowIdxBase

uint32_t EthRemoteCfg_AllocRxRes::rxFlowIdxBase

Allocated Rx flow index base.

◆ rxFlowIdxOffset

uint32_t EthRemoteCfg_AllocRxRes::rxFlowIdxOffset

Allocated flow index offset.

◆ rxPsilSrcId

uint32_t EthRemoteCfg_AllocRxRes::rxPsilSrcId

Rx PSIL peer source thread id