ETHFW API Guide
|
Ethernet Firmware version.
Version of the Ethernet Firmware.
Data Fields | |
uint32_t | major |
uint32_t | minor |
uint32_t | rev |
int8_t | year [ETHFW_VERSION_YEARLEN+1U] |
int8_t | month [ETHFW_VERSION_MONTHLEN+1U] |
int8_t | date [ETHFW_VERSION_DATELEN+1U] |
int8_t | hour [ETHFW_VERSION_HOURLEN+1U] |
int8_t | min [ETHFW_VERSION_MINLEN+1U] |
int8_t | sec [ETHFW_VERSION_SECLEN+1U] |
int8_t | commitHash [ETHFW_VERSION_COMMITSHALEN+1U] |
uint32_t EthFw_Version::major |
Major version number
uint32_t EthFw_Version::minor |
Minor version number
uint32_t EthFw_Version::rev |
Revision version number
int8_t EthFw_Version::year[ETHFW_VERSION_YEARLEN+1U] |
Remote Ethernet Switch Device Firmware Build year: char string in the form YYYY eg: 2019
int8_t EthFw_Version::month[ETHFW_VERSION_MONTHLEN+1U] |
Remote Ethernet Switch Device Firmware Build month: char string in the form MON eg: Dec
int8_t EthFw_Version::date[ETHFW_VERSION_DATELEN+1U] |
Remote Ethernet Switch Device Firmware Build date: char string in the form DD eg: 12
int8_t EthFw_Version::hour[ETHFW_VERSION_HOURLEN+1U] |
Remote Ethernet Switch Device Firmware Build hour in 24 hour format
int8_t EthFw_Version::min[ETHFW_VERSION_MINLEN+1U] |
Remote Ethernet Switch Device Firmware Build minute
int8_t EthFw_Version::sec[ETHFW_VERSION_SECLEN+1U] |
Remote Ethernet Switch Device Firmware Build second
int8_t EthFw_Version::commitHash[ETHFW_VERSION_COMMITSHALEN+1U] |
GIT commit SHA of the firmware: char string in the form fd52c34f