ETHFW API Guide
|
Static VLAN configuration.
Data Fields | |
const EthFwVlan_VlanCfg * | vlanCfg |
uint32_t | numVlans |
uint32_t | dfltVlanIdSwitchPorts |
uint32_t | dfltVlanIdMacOnlyPorts |
uint32_t | switchPortMask |
uint32_t | macOnlyPortMask |
const EthFwVlan_VlanCfg* EthFwVlan_Cfg::vlanCfg |
Pointer to the static VLANs parameters
uint32_t EthFwVlan_Cfg::numVlans |
Number of static VLANs in EthFwVlan_Cfg::vlanCfg
uint32_t EthFwVlan_Cfg::dfltVlanIdSwitchPorts |
Default VLAN id used by Ethernet Firmware for switch ports (non MAC-only)
uint32_t EthFwVlan_Cfg::dfltVlanIdMacOnlyPorts |
Default VLAN id used by Ethernet Firmware for MAC-only ports
uint32_t EthFwVlan_Cfg::switchPortMask |
Port mask of ports in switch mode (non MAC-only)
uint32_t EthFwVlan_Cfg::macOnlyPortMask |
Port mask of ports in MAC-only mode