CC3000
1.14
|
Functions | |
INT32 | nvmem_read (UINT32 ulFileId, UINT32 ulLength, UINT32 ulOffset, UINT8 *buff) |
Reads data from the file referred by the ulFileId parameter. Reads data from file ulOffset till length. Err if the file can't be used, is invalid, or if the read is out of bounds. More... | |
INT32 | nvmem_write (UINT32 ulFileId, UINT32 ulLength, UINT32 ulEntryOffset, UINT8 *buff) |
Write data to nvmem. writes data to file referred by the ulFileId parameter. Writes data to file ulOffset till ulLength.The file id will be marked invalid till the write is done. The file entry doesn't need to be valid - only allocated. More... | |
UINT8 | nvmem_set_mac_address (UINT8 *mac) |
Write MAC address to EEPROM. mac address as appears over the air (OUI first) More... | |
UINT8 | nvmem_get_mac_address (UINT8 *mac) |
Read MAC address from EEPROM. mac address as appears over the air (OUI first) More... | |
UINT8 | nvmem_write_patch (UINT32 ulFileId, UINT32 spLength, const UINT8 *spData) |
program a patch to a specific file ID. The SP data is assumed to be organized in 2-dimensional. Each line is SP_PORTION_SIZE bytes long. Actual programming is applied in SP_PORTION_SIZE bytes portions. More... | |
UINT8 | nvmem_read_sp_version (UINT8 *patchVer) |
Read patch version. read package version (WiFi FW patch, driver-supplicant-NS patch, bootloader patch) More... | |
INT32 | nvmem_create_entry (UINT32 ulFileId, UINT32 ulNewLen) |
Create new file entry and allocate space on the NVMEM. Applies only to user files. Modify the size of file. If the entry is unallocated - allocate it to size ulNewLen (marked invalid). If it is allocated then deallocate it first. To just mark the file as invalid without resizing - set ulNewLen=0. More... | |
INT32 nvmem_create_entry | ( | UINT32 | ulFileId, |
UINT32 | ulNewLen | ||
) |
Create new file entry and allocate space on the NVMEM. Applies only to user files. Modify the size of file. If the entry is unallocated - allocate it to size ulNewLen (marked invalid). If it is allocated then deallocate it first. To just mark the file as invalid without resizing - set ulNewLen=0.
nvmem_create_entry
ulFileId | nvmem file Id:
|
ulNewLen | entry ulLength |
UINT8 nvmem_get_mac_address | ( | UINT8 * | mac | ) |
Read MAC address from EEPROM. mac address as appears over the air (OUI first)
nvmem_get_mac_address
[out] | mac | mac address |
INT32 nvmem_read | ( | UINT32 | ulFileId, |
UINT32 | ulLength, | ||
UINT32 | ulOffset, | ||
UINT8 * | buff | ||
) |
Reads data from the file referred by the ulFileId parameter. Reads data from file ulOffset till length. Err if the file can't be used, is invalid, or if the read is out of bounds.
nvmem_read
ulFileId | nvmem file id: NVMEM_NVS_FILEID, NVMEM_NVS_SHADOW_FILEID, NVMEM_WLAN_CONFIG_FILEID, NVMEM_WLAN_CONFIG_SHADOW_FILEID, NVMEM_WLAN_DRIVER_SP_FILEID, NVMEM_WLAN_FW_SP_FILEID, NVMEM_MAC_FILEID, NVMEM_FRONTEND_VARS_FILEID, NVMEM_IP_CONFIG_FILEID, NVMEM_IP_CONFIG_SHADOW_FILEID, NVMEM_BOOTLOADER_SP_FILEID, NVMEM_RM_FILEID, and user files 12-15. |
ulLength | number of bytes to read |
ulOffset | ulOffset in file from where to read |
buff | output buffer pointer |
UINT8 nvmem_read_sp_version | ( | UINT8 * | patchVer | ) |
Read patch version. read package version (WiFi FW patch, driver-supplicant-NS patch, bootloader patch)
nvmem_read_sp_version
[out] | patchVer | first number indicates package ID and the second number indicates package build number |
UINT8 nvmem_set_mac_address | ( | UINT8 * | mac | ) |
Write MAC address to EEPROM. mac address as appears over the air (OUI first)
nvmem_set_mac_address
mac | mac address to be set |
INT32 nvmem_write | ( | UINT32 | ulFileId, |
UINT32 | ulLength, | ||
UINT32 | ulEntryOffset, | ||
UINT8 * | buff | ||
) |
Write data to nvmem. writes data to file referred by the ulFileId parameter. Writes data to file ulOffset till ulLength.The file id will be marked invalid till the write is done. The file entry doesn't need to be valid - only allocated.
nvmem_write
ulFileId | nvmem file id: NVMEM_WLAN_DRIVER_SP_FILEID, NVMEM_WLAN_FW_SP_FILEID, NVMEM_MAC_FILEID, NVMEM_BOOTLOADER_SP_FILEID, and user files 12-15. |
ulLength | number of bytes to write |
ulEntryOffset | offset in file to start write operation from |
buff | data to write |
UINT8 nvmem_write_patch | ( | UINT32 | ulFileId, |
UINT32 | spLength, | ||
const UINT8 * | spData | ||
) |
program a patch to a specific file ID. The SP data is assumed to be organized in 2-dimensional. Each line is SP_PORTION_SIZE bytes long. Actual programming is applied in SP_PORTION_SIZE bytes portions.
nvmem_write_patch
ulFileId | nvmem file id: NVMEM_WLAN_DRIVER_SP_FILEID, NVMEM_WLAN_FW_SP_FILEID, |
spLength | number of bytes to write |
spData | SP data to write |