CC3000  1.12
 All Classes Functions Groups
sSimplLinkInformation Struct Reference

Public Attributes

UINT16 usRxEventOpcode
 
UINT16 usEventOrDataReceived
 
UINT8 * pucReceivedData
 
UINT8 * pucTxCommandBuffer
 
tFWPatches sFWPatches
 
tDriverPatches sDriverPatches
 
tBootLoaderPatches sBootLoaderPatches
 
tWlanCB sWlanCB
 
tWlanReadInteruptPin ReadWlanInterruptPin
 
tWlanInterruptEnable WlanInterruptEnable
 
tWlanInterruptDisable WlanInterruptDisable
 
tWriteWlanPin WriteWlanPin
 
INT32 slTransmitDataError
 
UINT16 usNumberOfFreeBuffers
 
UINT16 usSlBufferLength
 
UINT16 usBufferSize
 
UINT16 usRxDataPending
 
UINT32 NumberOfSentPackets
 
UINT32 NumberOfReleasedPackets
 
UINT8 InformHostOnTxComplete
 

The documentation for this struct was generated from the following file: