CC3000  1.12
 All Classes Functions Groups
Socket_api

Classes

struct  _in_addr_t
 
struct  _sockaddr_t
 
struct  _sockaddr_in_t
 
struct  fd_set
 

Macros

#define SOCKET_OPEN_PARAMS_LEN   (12)
 
#define SOCKET_CLOSE_PARAMS_LEN   (4)
 
#define SOCKET_ACCEPT_PARAMS_LEN   (4)
 
#define SOCKET_BIND_PARAMS_LEN   (20)
 
#define SOCKET_LISTEN_PARAMS_LEN   (8)
 
#define SOCKET_GET_HOST_BY_NAME_PARAMS_LEN   (9)
 
#define SOCKET_CONNECT_PARAMS_LEN   (20)
 
#define SOCKET_SELECT_PARAMS_LEN   (44)
 
#define SOCKET_SET_SOCK_OPT_PARAMS_LEN   (20)
 
#define SOCKET_GET_SOCK_OPT_PARAMS_LEN   (12)
 
#define SOCKET_RECV_FROM_PARAMS_LEN   (12)
 
#define SOCKET_SENDTO_PARAMS_LEN   (24)
 
#define SOCKET_MDNS_ADVERTISE_PARAMS_LEN   (12)
 
#define SOCKET_GET_MSS_VALUE_PARAMS_LEN   (4)
 
#define HCI_CMND_SEND_ARG_LENGTH   (16)
 
#define SELECT_TIMEOUT_MIN_MICRO_SECONDS   5000
 
#define HEADERS_SIZE_DATA   (SPI_HEADER_SIZE + 5)
 
#define SIMPLE_LINK_HCI_CMND_TRANSPORT_HEADER_SIZE   (SPI_HEADER_SIZE + SIMPLE_LINK_HCI_CMND_HEADER_SIZE)
 
#define MDNS_DEVICE_SERVICE_MAX_LENGTH   (32)
 
#define HOSTNAME_MAX_LENGTH   (230)
 
#define AF_INET   2
 
#define AF_INET6   23
 
#define SOCK_STREAM   1
 
#define SOCK_DGRAM   2
 
#define SOCK_RAW   3
 
#define SOCK_RDM   4
 
#define SOCK_SEQPACKET   5
 
#define IPPROTO_IP   0
 
#define IPPROTO_ICMP   1
 
#define IPPROTO_IPV4   IPPROTO_IP
 
#define IPPROTO_TCP   6
 
#define IPPROTO_UDP   17
 
#define IPPROTO_IPV6   41
 
#define IPPROTO_NONE   59
 
#define IPPROTO_RAW   255
 
#define IPPROTO_MAX   256
 
#define SOC_ERROR   (-1)
 
#define SOC_IN_PROGRESS   (-2)
 
#define SOL_SOCKET   0xffff
 
#define SOCKOPT_RECV_NONBLOCK   0
 
#define SOCKOPT_RECV_TIMEOUT   1
 
#define SOCKOPT_ACCEPT_NONBLOCK   2
 
#define SOCK_ON   0
 
#define SOCK_OFF   1
 
#define MAX_PACKET_SIZE   1500
 
#define MAX_LISTEN_QUEUE   4
 
#define IOCTL_SOCKET_EVENTMASK
 
#define ENOBUFS   55
 
#define __FD_SETSIZE   32
 
#define ASIC_ADDR_LEN   8
 
#define NO_QUERY_RECIVED   -3
 
#define __NFDBITS   (8 * sizeof (__fd_mask))
 
#define __FDELT(d)   ((d) / __NFDBITS)
 
#define __FDMASK(d)   ((__fd_mask) 1 << ((d) % __NFDBITS))
 
#define __FD_ZERO(set)
 
#define __FD_SET(d, set)   (__FDS_BITS (set)[__FDELT (d)] |= __FDMASK (d))
 
#define __FD_CLR(d, set)   (__FDS_BITS (set)[__FDELT (d)] &= ~__FDMASK (d))
 
#define __FD_ISSET(d, set)   (__FDS_BITS (set)[__FDELT (d)] & __FDMASK (d))
 
#define FD_SET(fd, fdsetp)   __FD_SET (fd, fdsetp)
 
#define FD_CLR(fd, fdsetp)   __FD_CLR (fd, fdsetp)
 
#define FD_ISSET(fd, fdsetp)   __FD_ISSET (fd, fdsetp)
 
#define FD_ZERO(fdsetp)   __FD_ZERO (fdsetp)
 
#define htonl(A)
 
#define ntohl   htonl
 
#define htons(A)
 
#define ntohs   htons
 
#define SET_mDNS_ADD(sockaddr)
 

Typedefs

typedef struct _in_addr_t in_addr
 
typedef struct _sockaddr_t sockaddr
 
typedef struct _sockaddr_in_t sockaddr_in
 
typedef UINT32 socklen_t
 
typedef INT32 __fd_mask
 

Functions

INT16 HostFlowControlConsumeBuff (INT16 sd)
 if SEND_NON_BLOCKING not define - block until have free buffer becomes available, else return immediately with correct status regarding the buffers available. More...
 
INT16 socket (INT32 domain, INT32 type, INT32 protocol)
 create an endpoint for communication The socket function creates a socket that is bound to a specific transport service provider. This function is called by the application layer to obtain a socket handle. More...
 
INT32 closesocket (INT32 sd)
 The socket function closes a created socket. More...
 
INT32 accept (INT32 sd, sockaddr *addr, socklen_t *addrlen)
 accept a connection on a socket: This function is used with connection-based socket types (SOCK_STREAM). It extracts the first connection request on the queue of pending connections, creates a new connected socket, and returns a new file descriptor referring to that socket. The newly created socket is not in the listening state. The original socket sd is unaffected by this call. The argument sd is a socket that has been created with socket(), bound to a local address with bind(), and is listening for connections after a listen(). The argument addr is a pointer to a sockaddr structure. This structure is filled in with the address of the peer socket, as known to the communications layer. The exact format of the address returned addr is determined by the socket's address family. The addrlen argument is a value-result argument: it should initially contain the size of the structure pointed to by addr, on return it will contain the actual length (in bytes) of the address returned. More...
 
INT32 bind (INT32 sd, const sockaddr *addr, INT32 addrlen)
 assign a name to a socket This function gives the socket the local address addr. addr is addrlen bytes long. Traditionally, this is called when a socket is created with socket, it exists in a name space (address family) but has no name assigned. It is necessary to assign a local address before a SOCK_STREAM socket may receive connections. More...
 
INT32 listen (INT32 sd, INT32 backlog)
 listen for connections on a socket The willingness to accept incoming connections and a queue limit for incoming connections are specified with listen(), and then the connections are accepted with accept. The listen() call applies only to sockets of type SOCK_STREAM The backlog parameter defines the maximum length the queue of pending connections may grow to. More...
 
INT16 gethostbyname (CHAR *hostname, UINT16 usNameLen, UINT32 *out_ip_addr)
 Get host IP by name. Obtain the IP Address of machine on network, by its name. More...
 
INT32 connect (INT32 sd, const sockaddr *addr, INT32 addrlen)
 initiate a connection on a socket Function connects the socket referred to by the socket descriptor sd, to the address specified by addr. The addrlen argument specifies the size of addr. The format of the address in addr is determined by the address space of the socket. If it is of type SOCK_DGRAM, this call specifies the peer with which the socket is to be associated; this address is that to which datagrams are to be sent, and the only address from which datagrams are to be received. If the socket is of type SOCK_STREAM, this call attempts to make a connection to another socket. The other socket is specified by address, which is an address in the communications space of the socket. Note that the function implements only blocking behavior thus the caller will be waiting either for the connection establishment or for the connection establishment failure. More...
 
INT16 select (INT32 nfds, fd_set *readsds, fd_set *writesds, fd_set *exceptsds, struct timeval *timeout)
 Monitor socket activity Select allow a program to monitor multiple file descriptors, waiting until one or more of the file descriptors become "ready" for some class of I/O operation. More...
 
INT16 setsockopt (INT32 sd, INT32 level, INT32 optname, const void *optval, socklen_t optlen)
 set socket options This function manipulate the options associated with a socket. Options may exist at multiple protocol levels; they are always present at the uppermost socket level. When manipulating socket options the level at which the option resides and the name of the option must be specified. To manipulate options at the socket level, level is specified as SOL_SOCKET. To manipulate options at any other level the protocol number of the appropriate protocol controlling the option is supplied. For example, to indicate that an option is to be interpreted by the TCP protocol, level should be set to the protocol number of TCP; The parameters optval and optlen are used to access optval - use for setsockopt(). For getsockopt() they identify a buffer in which the value for the requested option(s) are to be returned. For getsockopt(), optlen is a value-result parameter, initially containing the size of the buffer pointed to by option_value, and modified on return to indicate the actual size of the value returned. If no option value is to be supplied or returned, option_value may be NULL. More...
 
INT16 getsockopt (INT32 sd, INT32 level, INT32 optname, void *optval, socklen_t *optlen)
 set socket options This function manipulate the options associated with a socket. Options may exist at multiple protocol levels; they are always present at the uppermost socket level. When manipulating socket options the level at which the option resides and the name of the option must be specified. To manipulate options at the socket level, level is specified as SOL_SOCKET. To manipulate options at any other level the protocol number of the appropriate protocol controlling the option is supplied. For example, to indicate that an option is to be interpreted by the TCP protocol, level should be set to the protocol number of TCP; The parameters optval and optlen are used to access optval - use for setsockopt(). For getsockopt() they identify a buffer in which the value for the requested option(s) are to be returned. For getsockopt(), optlen is a value-result parameter, initially containing the size of the buffer pointed to by option_value, and modified on return to indicate the actual size of the value returned. If no option value is to be supplied or returned, option_value may be NULL. More...
 
INT16 simple_link_recv (INT32 sd, void *buf, INT32 len, INT32 flags, sockaddr *from, socklen_t *fromlen, INT32 opcode)
 Read data from socket Return the length of the message on successful completion. If a message is too long to fit in the supplied buffer, excess bytes may be discarded depending on the type of socket the message is received from. More...
 
INT16 recv (INT32 sd, void *buf, INT32 len, INT32 flags)
 function receives a message from a connection-mode socket More...
 
INT16 recvfrom (INT32 sd, void *buf, INT32 len, INT32 flags, sockaddr *from, socklen_t *fromlen)
 read data from socket function receives a message from a connection-mode or connectionless-mode socket. Note that raw sockets are not supported. More...
 
INT16 simple_link_send (INT32 sd, const void *buf, INT32 len, INT32 flags, const sockaddr *to, INT32 tolen, INT32 opcode)
 This function is used to transmit a message to another socket. More...
 
INT16 send (INT32 sd, const void *buf, INT32 len, INT32 flags)
 Write data to TCP socket This function is used to transmit a message to another socket. More...
 
INT16 sendto (INT32 sd, const void *buf, INT32 len, INT32 flags, const sockaddr *to, socklen_t tolen)
 Write data to TCP socket This function is used to transmit a message to another socket. More...
 
INT16 mdnsAdvertiser (UINT16 mdnsEnabled, CHAR *deviceServiceName, UINT16 deviceServiceNameLength)
 Set CC3000 in mDNS advertiser mode in order to advertise itself. More...
 
UINT16 getmssvalue (INT32 sd)
 Returns the MSS value of a TCP connection according to the socket descriptor. More...
 

Detailed Description

Macro Definition Documentation

#define __FD_ZERO (   set)
Value:
do { \
UINT16 __i; \
fd_set *__arr = (set); \
for (__i = 0; __i < sizeof (fd_set) / sizeof (__fd_mask); ++__i) \
__FDS_BITS (__arr)[__i] = 0; \
} while (0)
Definition: socket.h:141
#define htonl (   A)
Value:
((((UINT32)(A) & 0xff000000) >> 24) | \
(((UINT32)(A) & 0x00ff0000) >> 8) | \
(((UINT32)(A) & 0x0000ff00) << 8) | \
(((UINT32)(A) & 0x000000ff) << 24))
#define htons (   A)
Value:
((((UINT32)(A) & 0xff00) >> 8) | \
(((UINT32)(A) & 0x00ff) << 8))
#define SET_mDNS_ADD (   sockaddr)
Value:
sockaddr.sa_data[0] = 0x14; \
sockaddr.sa_data[1] = 0xe9; \
sockaddr.sa_data[2] = 0xe0; \
sockaddr.sa_data[3] = 0x0; \
sockaddr.sa_data[4] = 0x0; \
sockaddr.sa_data[5] = 0xfb;
Definition: socket.h:116

Function Documentation

INT32 accept ( INT32  sd,
sockaddr *  addr,
socklen_t *  addrlen 
)

accept a connection on a socket: This function is used with connection-based socket types (SOCK_STREAM). It extracts the first connection request on the queue of pending connections, creates a new connected socket, and returns a new file descriptor referring to that socket. The newly created socket is not in the listening state. The original socket sd is unaffected by this call. The argument sd is a socket that has been created with socket(), bound to a local address with bind(), and is listening for connections after a listen(). The argument addr is a pointer to a sockaddr structure. This structure is filled in with the address of the peer socket, as known to the communications layer. The exact format of the address returned addr is determined by the socket's address family. The addrlen argument is a value-result argument: it should initially contain the size of the structure pointed to by addr, on return it will contain the actual length (in bytes) of the address returned.

accept

Parameters
[in]sdsocket descriptor (handle)
[out]addrthe argument addr is a pointer to a sockaddr structure This structure is filled in with the address of the peer socket, as known to the communications layer. determined. The exact format of the address returned addr is by the socket's address sockaddr. On this version only AF_INET is supported. This argument returns in network order.
[out]addrlenthe addrlen argument is a value-result argument: it should initially contain the size of the structure pointed to by addr.
Returns
For socket in blocking mode: On success, socket handle. on failure negative For socket in non-blocking mode:
  • On connection establishment, socket handle
  • On connection pending, SOC_IN_PROGRESS (-2)
  • On failure, SOC_ERROR (-1)
See Also
socket ; bind ; listen
INT32 bind ( INT32  sd,
const sockaddr *  addr,
INT32  addrlen 
)

assign a name to a socket This function gives the socket the local address addr. addr is addrlen bytes long. Traditionally, this is called when a socket is created with socket, it exists in a name space (address family) but has no name assigned. It is necessary to assign a local address before a SOCK_STREAM socket may receive connections.

bind

Parameters
[in]sdsocket descriptor (handle)
[out]addrspecifies the destination address. On this version only AF_INET is supported.
[out]addrlencontains the size of the structure pointed to by addr.
Returns
On success, zero is returned. On error, -1 is returned.
See Also
socket ; accept ; listen
INT32 closesocket ( INT32  sd)

The socket function closes a created socket.

closesocket

Parameters
sdsocket handle.
Returns
On success, zero is returned. On error, -1 is returned.
INT32 connect ( INT32  sd,
const sockaddr *  addr,
INT32  addrlen 
)

initiate a connection on a socket Function connects the socket referred to by the socket descriptor sd, to the address specified by addr. The addrlen argument specifies the size of addr. The format of the address in addr is determined by the address space of the socket. If it is of type SOCK_DGRAM, this call specifies the peer with which the socket is to be associated; this address is that to which datagrams are to be sent, and the only address from which datagrams are to be received. If the socket is of type SOCK_STREAM, this call attempts to make a connection to another socket. The other socket is specified by address, which is an address in the communications space of the socket. Note that the function implements only blocking behavior thus the caller will be waiting either for the connection establishment or for the connection establishment failure.

connect

Parameters
[in]sdsocket descriptor (handle)
[in]addrspecifies the destination addr. On this version only AF_INET is supported.
[out]addrlencontains the size of the structure pointed to by addr
Returns
On success, zero is returned. On error, -1 is returned
See Also
socket
INT16 gethostbyname ( CHAR *  hostname,
UINT16  usNameLen,
UINT32 *  out_ip_addr 
)

Get host IP by name. Obtain the IP Address of machine on network, by its name.

gethostbyname

Parameters
[in]hostnamehost name
[in]usNameLenname length
[out]out_ip_addrThis parameter is filled in with host IP address. In case that host name is not resolved, out_ip_addr is zero.
Returns
On success, positive is returned. On error, negative is returned
Note
On this version, only blocking mode is supported. Also note that the function requires DNS server to be configured prior to its usage.
UINT16 getmssvalue ( INT32  sd)

Returns the MSS value of a TCP connection according to the socket descriptor.

getmssvalue

Parameters
[in]sdsocket descriptor
Returns
On success, returns the MSS value of a TCP connection
INT16 getsockopt ( INT32  sd,
INT32  level,
INT32  optname,
void *  optval,
socklen_t *  optlen 
)

set socket options This function manipulate the options associated with a socket. Options may exist at multiple protocol levels; they are always present at the uppermost socket level. When manipulating socket options the level at which the option resides and the name of the option must be specified. To manipulate options at the socket level, level is specified as SOL_SOCKET. To manipulate options at any other level the protocol number of the appropriate protocol controlling the option is supplied. For example, to indicate that an option is to be interpreted by the TCP protocol, level should be set to the protocol number of TCP; The parameters optval and optlen are used to access optval - use for setsockopt(). For getsockopt() they identify a buffer in which the value for the requested option(s) are to be returned. For getsockopt(), optlen is a value-result parameter, initially containing the size of the buffer pointed to by option_value, and modified on return to indicate the actual size of the value returned. If no option value is to be supplied or returned, option_value may be NULL.

getsockopt

Parameters
[in]sdsocket handle
[in]leveldefines the protocol level for this option
[in]optnamedefines the option name to Interrogate
[out]optvalspecifies a value for the option
[out]optlenspecifies the length of the option value
Returns
On success, zero is returned. On error, -1 is returned

On this version the following two socket options are enabled: The only protocol level supported in this version is SOL_SOCKET (level).

  1. SOCKOPT_RECV_TIMEOUT (optname) SOCKOPT_RECV_TIMEOUT configures recv and recvfrom timeout in milliseconds. In that case optval should be pointer to UINT32.
  2. SOCKOPT_NONBLOCK (optname). sets the socket non-blocking mode on or off. In that case optval should be SOCK_ON or SOCK_OFF (optval).
See Also
setsockopt
INT16 HostFlowControlConsumeBuff ( INT16  sd)

if SEND_NON_BLOCKING not define - block until have free buffer becomes available, else return immediately with correct status regarding the buffers available.

HostFlowControlConsumeBuff

Parameters
sdsocket descriptor
Returns
0 in case there are buffers available, -1 in case of bad socket -2 if there are no free buffers present (only when SEND_NON_BLOCKING is enabled)
INT32 listen ( INT32  sd,
INT32  backlog 
)

listen for connections on a socket The willingness to accept incoming connections and a queue limit for incoming connections are specified with listen(), and then the connections are accepted with accept. The listen() call applies only to sockets of type SOCK_STREAM The backlog parameter defines the maximum length the queue of pending connections may grow to.

listen

Parameters
[in]sdsocket descriptor (handle)
[in]backlogspecifies the listen queue depth. On this version backlog is not supported.
Returns
On success, zero is returned. On error, -1 is returned.
See Also
socket ; accept ; bind
Note
On this version, backlog is not supported
INT16 mdnsAdvertiser ( UINT16  mdnsEnabled,
CHAR *  deviceServiceName,
UINT16  deviceServiceNameLength 
)

Set CC3000 in mDNS advertiser mode in order to advertise itself.

mdnsAdvertiser

Parameters
[in]mdnsEnabledflag to enable/disable the mDNS feature
[in]deviceServiceNameService name as part of the published canonical domain name
[in]deviceServiceNameLengthLength of the service name - up to 32 chars
Returns
On success, zero is returned, return SOC_ERROR if socket was not opened successfully, or if an error occurred.
INT16 recv ( INT32  sd,
void *  buf,
INT32  len,
INT32  flags 
)

function receives a message from a connection-mode socket

recv

Parameters
[in]sdsocket handle
[out]bufPoints to the buffer where the message should be stored
[in]lenSpecifies the length in bytes of the buffer pointed to by the buffer argument.
[in]flagsSpecifies the type of message reception. On this version, this parameter is not supported.
Returns
Return the number of bytes received, or -1 if an error occurred
See Also
recvfrom

On this version, only blocking mode is supported.

INT16 recvfrom ( INT32  sd,
void *  buf,
INT32  len,
INT32  flags,
sockaddr *  from,
socklen_t *  fromlen 
)

read data from socket function receives a message from a connection-mode or connectionless-mode socket. Note that raw sockets are not supported.

recvfrom

Parameters
[in]sdsocket handle
[out]bufPoints to the buffer where the message should be stored
[in]lenSpecifies the length in bytes of the buffer pointed to by the buffer argument.
[in]flagsSpecifies the type of message reception. On this version, this parameter is not supported.
[in]frompointer to an address structure indicating the source address: sockaddr. On this version only AF_INET is supported.
[in]fromlensource address tructure size
Returns
Return the number of bytes received, or -1 if an error occurred
See Also
recv

On this version, only blocking mode is supported.

recvfrom

Parameters
[in]sdsocket handle
[out]bufPoints to the buffer where the message should be stored
[in]lenSpecifies the length in bytes of the buffer pointed to by the buffer argument.
[in]flagsSpecifies the type of message reception. On this version, this parameter is not supported.
[in]frompointer to an address structure indicating the source address: sockaddr. On this version only AF_INET is supported.
[in]fromlensource address structure size
Returns
Return the number of bytes received, or -1 if an error occurred
See Also
recv

On this version, only blocking mode is supported.

INT16 select ( INT32  nfds,
fd_set *  readsds,
fd_set *  writesds,
fd_set *  exceptsds,
struct timeval *  timeout 
)

Monitor socket activity Select allow a program to monitor multiple file descriptors, waiting until one or more of the file descriptors become "ready" for some class of I/O operation.

select

Parameters
[in]nfdsthe highest-numbered file descriptor in any of the three sets, plus 1.
[out]writesdssocket descriptors list for write monitoring
[out]readsdssocket descriptors list for read monitoring
[out]exceptsdssocket descriptors list for exception monitoring
[in]timeoutis an upper bound on the amount of time elapsed before select() returns. Null means infinity timeout. The minimum timeout is 5 milliseconds, less than 5 milliseconds will be set automatically to 5 milliseconds.
Returns
On success, select() returns the number of file descriptors contained in the three returned descriptor sets (that is, the total number of bits that are set in readfds, writefds, exceptfds) which may be zero if the timeout expires before anything interesting happens. On error, -1 is returned. *readsds - return the sockets on which Read request will return without delay with valid data. *writesds - return the sockets on which Write request will return without delay. *exceptsds - return the sockets which closed recently.

If the timeout value set to less than 5ms it will automatically set to 5ms to prevent overload of the system

See Also
socket
INT16 send ( INT32  sd,
const void *  buf,
INT32  len,
INT32  flags 
)

Write data to TCP socket This function is used to transmit a message to another socket.

send

Parameters
sdsocket handle
bufPoints to a buffer containing the message to be sent
lenmessage size in bytes
flagsOn this version, this parameter is not supported
Returns
Return the number of bytes transmitted, or -1 if an error occurred

On this version, only blocking mode is supported.

See Also
sendto
INT16 sendto ( INT32  sd,
const void *  buf,
INT32  len,
INT32  flags,
const sockaddr *  to,
socklen_t  tolen 
)

Write data to TCP socket This function is used to transmit a message to another socket.

sendto

Parameters
sdsocket handle
bufPoints to a buffer containing the message to be sent
lenmessage size in bytes
flagsOn this version, this parameter is not supported
topointer to an address structure indicating the destination address: sockaddr. On this version only AF_INET is supported.
tolendestination address structure size
Returns
Return the number of bytes transmitted, or -1 if an error occurred

On this version, only blocking mode is supported.

See Also
send
INT16 setsockopt ( INT32  sd,
INT32  level,
INT32  optname,
const void *  optval,
socklen_t  optlen 
)

set socket options This function manipulate the options associated with a socket. Options may exist at multiple protocol levels; they are always present at the uppermost socket level. When manipulating socket options the level at which the option resides and the name of the option must be specified. To manipulate options at the socket level, level is specified as SOL_SOCKET. To manipulate options at any other level the protocol number of the appropriate protocol controlling the option is supplied. For example, to indicate that an option is to be interpreted by the TCP protocol, level should be set to the protocol number of TCP; The parameters optval and optlen are used to access optval - use for setsockopt(). For getsockopt() they identify a buffer in which the value for the requested option(s) are to be returned. For getsockopt(), optlen is a value-result parameter, initially containing the size of the buffer pointed to by option_value, and modified on return to indicate the actual size of the value returned. If no option value is to be supplied or returned, option_value may be NULL.

setsockopt

Parameters
[in]sdsocket handle
[in]leveldefines the protocol level for this option
[in]optnamedefines the option name to Interrogate
[in]optvalspecifies a value for the option
[in]optlenspecifies the length of the option value
Returns
On success, zero is returned. On error, -1 is returned

On this version the following two socket options are enabled: The only protocol level supported in this version is SOL_SOCKET (level).

  1. SOCKOPT_RECV_TIMEOUT (optname) SOCKOPT_RECV_TIMEOUT configures recv and recvfrom timeout in milliseconds. In that case optval should be pointer to UINT32.
  2. SOCKOPT_NONBLOCK (optname). sets the socket non-blocking mode on or off. In that case optval should be SOCK_ON or SOCK_OFF (optval).
See Also
getsockopt
INT16 simple_link_recv ( INT32  sd,
void *  buf,
INT32  len,
INT32  flags,
sockaddr *  from,
socklen_t *  fromlen,
INT32  opcode 
)

Read data from socket Return the length of the message on successful completion. If a message is too long to fit in the supplied buffer, excess bytes may be discarded depending on the type of socket the message is received from.

simple_link_recv

Parameters
sdsocket handle
bufread buffer
lenbuffer length
flagsindicates blocking or non-blocking operation
frompointer to an address structure indicating source address
fromlensource address structure size
Returns
Return the number of bytes received, or -1 if an error occurred
INT16 simple_link_send ( INT32  sd,
const void *  buf,
INT32  len,
INT32  flags,
const sockaddr *  to,
INT32  tolen,
INT32  opcode 
)

This function is used to transmit a message to another socket.

simple_link_send

Parameters
sdsocket handle
bufwrite buffer
lenbuffer length
flagsOn this version, this parameter is not supported
topointer to an address structure indicating destination address
tolendestination address structure size
Returns
Return the number of bytes transmitted, or -1 if an error occurred, or -2 in case there are no free buffers available (only when SEND_NON_BLOCKING is enabled)
INT16 socket ( INT32  domain,
INT32  type,
INT32  protocol 
)

create an endpoint for communication The socket function creates a socket that is bound to a specific transport service provider. This function is called by the application layer to obtain a socket handle.

socket

Parameters
domainselects the protocol family which will be used for communication. On this version only AF_INET is supported
typespecifies the communication semantics. On this version only SOCK_STREAM, SOCK_DGRAM, SOCK_RAW are supported
protocolspecifies a particular protocol to be used with the socket IPPROTO_TCP, IPPROTO_UDP or IPPROTO_RAW are supported.
Returns
On success, socket handle that is used for consequent socket operations. On error, -1 is returned.