CC3000  1.12
 All Classes Functions Groups
Security_api

Functions

void expandKey (UINT8 *expandedKey, UINT8 *key)
 expend a 16 bytes key for AES128 implementation More...
 
UINT8 galois_mul2 (UINT8 value)
 multiply by 2 in the galois field More...
 
void aes_encr (UINT8 *state, UINT8 *expandedKey)
 internal implementation of AES128 encryption. straight forward aes encryption implementation first the group of operations More...
 
void aes_decr (UINT8 *state, UINT8 *expandedKey)
 internal implementation of AES128 decryption. straight forward aes decryption implementation the order of substeps is the exact reverse of decryption inverse functions: More...
 
void aes_encrypt (UINT8 *state, UINT8 *key)
 AES128 encryption: Given AES128 key and 16 bytes plain text, cipher text of 16 bytes is computed. The AES implementation is in mode ECB (Electronic Code Book). More...
 
void aes_decrypt (UINT8 *state, UINT8 *key)
 AES128 decryption: Given AES128 key and 16 bytes cipher text, plain text of 16 bytes is computed The AES implementation is in mode ECB (Electronic Code Book). More...
 
INT32 aes_read_key (UINT8 *key)
 Reads AES128 key from EEPROM Reads the AES128 key from fileID #12 in EEPROM returns an error if the key does not exist. More...
 
INT32 aes_write_key (UINT8 *key)
 writes AES128 key from EEPROM Writes the AES128 key to fileID #12 in EEPROM More...
 

Variables

const UINT8 sbox [256]
 
const UINT8 rsbox [256]
 
const UINT8 Rcon [11]
 
UINT8 expandedKey [176]
 

Detailed Description

Function Documentation

void aes_decr ( UINT8 *  state,
UINT8 *  expandedKey 
)

internal implementation of AES128 decryption. straight forward aes decryption implementation the order of substeps is the exact reverse of decryption inverse functions:

aes_decr

Parameters
[in]expandedKeyexpanded AES128 key
in\out]state 16 bytes of cipher text and plain text
Returns
none
      - addRoundKey is its own inverse
      - rsbox is inverse of sbox
      - rightshift instead of leftshift
      - invMixColumns = barreto + mixColumns
     no further subfunctions to save cycles for function calls
     no structuring with "for (....)" to save cycles
void aes_decrypt ( UINT8 *  state,
UINT8 *  key 
)

AES128 decryption: Given AES128 key and 16 bytes cipher text, plain text of 16 bytes is computed The AES implementation is in mode ECB (Electronic Code Book).

aes_decrypt

Parameters
[in]keyAES128 key of size 16 bytes
in\out]state 16 bytes of cipher text and plain text
Returns
none
void aes_encr ( UINT8 *  state,
UINT8 *  expandedKey 
)

internal implementation of AES128 encryption. straight forward aes encryption implementation first the group of operations

aes_encr

Parameters
[in]expandedKeyexpanded AES128 key
in/out]state 16 bytes of plain text and cipher text
Returns
none
    - addRoundKey
    - subbytes
    - shiftrows
    - mixcolums
    is executed 9 times, after this addroundkey to finish the 9th 
    round, after that the 10th round without mixcolums
    no further subfunctions to save cycles for function calls
    no structuring with "for (....)" to save cycles.
void aes_encrypt ( UINT8 *  state,
UINT8 *  key 
)

AES128 encryption: Given AES128 key and 16 bytes plain text, cipher text of 16 bytes is computed. The AES implementation is in mode ECB (Electronic Code Book).

aes_encrypt

Parameters
[in]keyAES128 key of size 16 bytes
in\out]state 16 bytes of plain text and cipher text
Returns
none
INT32 aes_read_key ( UINT8 *  key)

Reads AES128 key from EEPROM Reads the AES128 key from fileID #12 in EEPROM returns an error if the key does not exist.

aes_read_key

Parameters
[out]keyAES128 key of size 16 bytes
Returns
on success 0, error otherwise.
INT32 aes_write_key ( UINT8 *  key)

writes AES128 key from EEPROM Writes the AES128 key to fileID #12 in EEPROM

aes_write_key

Parameters
[out]keyAES128 key of size 16 bytes
Returns
on success 0, error otherwise.
void expandKey ( UINT8 *  expandedKey,
UINT8 *  key 
)

expend a 16 bytes key for AES128 implementation

expandKey

Parameters
keyAES128 key - 16 bytes
expandedKeyexpanded AES128 key
Returns
none
UINT8 galois_mul2 ( UINT8  value)

multiply by 2 in the galois field

galois_mul2

Parameters
valueargument to multiply
Returns
multiplied argument

Variable Documentation

const UINT8 Rcon[11]
Initial value:
= {
0x8d, 0x01, 0x02, 0x04, 0x08, 0x10, 0x20, 0x40, 0x80, 0x1b, 0x36}
const UINT8 rsbox[256]
Initial value:
=
{ 0x52, 0x09, 0x6a, 0xd5, 0x30, 0x36, 0xa5, 0x38, 0xbf, 0x40, 0xa3, 0x9e, 0x81, 0xf3, 0xd7, 0xfb
, 0x7c, 0xe3, 0x39, 0x82, 0x9b, 0x2f, 0xff, 0x87, 0x34, 0x8e, 0x43, 0x44, 0xc4, 0xde, 0xe9, 0xcb
, 0x54, 0x7b, 0x94, 0x32, 0xa6, 0xc2, 0x23, 0x3d, 0xee, 0x4c, 0x95, 0x0b, 0x42, 0xfa, 0xc3, 0x4e
, 0x08, 0x2e, 0xa1, 0x66, 0x28, 0xd9, 0x24, 0xb2, 0x76, 0x5b, 0xa2, 0x49, 0x6d, 0x8b, 0xd1, 0x25
, 0x72, 0xf8, 0xf6, 0x64, 0x86, 0x68, 0x98, 0x16, 0xd4, 0xa4, 0x5c, 0xcc, 0x5d, 0x65, 0xb6, 0x92
, 0x6c, 0x70, 0x48, 0x50, 0xfd, 0xed, 0xb9, 0xda, 0x5e, 0x15, 0x46, 0x57, 0xa7, 0x8d, 0x9d, 0x84
, 0x90, 0xd8, 0xab, 0x00, 0x8c, 0xbc, 0xd3, 0x0a, 0xf7, 0xe4, 0x58, 0x05, 0xb8, 0xb3, 0x45, 0x06
, 0xd0, 0x2c, 0x1e, 0x8f, 0xca, 0x3f, 0x0f, 0x02, 0xc1, 0xaf, 0xbd, 0x03, 0x01, 0x13, 0x8a, 0x6b
, 0x3a, 0x91, 0x11, 0x41, 0x4f, 0x67, 0xdc, 0xea, 0x97, 0xf2, 0xcf, 0xce, 0xf0, 0xb4, 0xe6, 0x73
, 0x96, 0xac, 0x74, 0x22, 0xe7, 0xad, 0x35, 0x85, 0xe2, 0xf9, 0x37, 0xe8, 0x1c, 0x75, 0xdf, 0x6e
, 0x47, 0xf1, 0x1a, 0x71, 0x1d, 0x29, 0xc5, 0x89, 0x6f, 0xb7, 0x62, 0x0e, 0xaa, 0x18, 0xbe, 0x1b
, 0xfc, 0x56, 0x3e, 0x4b, 0xc6, 0xd2, 0x79, 0x20, 0x9a, 0xdb, 0xc0, 0xfe, 0x78, 0xcd, 0x5a, 0xf4
, 0x1f, 0xdd, 0xa8, 0x33, 0x88, 0x07, 0xc7, 0x31, 0xb1, 0x12, 0x10, 0x59, 0x27, 0x80, 0xec, 0x5f
, 0x60, 0x51, 0x7f, 0xa9, 0x19, 0xb5, 0x4a, 0x0d, 0x2d, 0xe5, 0x7a, 0x9f, 0x93, 0xc9, 0x9c, 0xef
, 0xa0, 0xe0, 0x3b, 0x4d, 0xae, 0x2a, 0xf5, 0xb0, 0xc8, 0xeb, 0xbb, 0x3c, 0x83, 0x53, 0x99, 0x61
, 0x17, 0x2b, 0x04, 0x7e, 0xba, 0x77, 0xd6, 0x26, 0xe1, 0x69, 0x14, 0x63, 0x55, 0x21, 0x0c, 0x7d }
const UINT8 sbox[256]
Initial value:
= {
0x63, 0x7c, 0x77, 0x7b, 0xf2, 0x6b, 0x6f, 0xc5, 0x30, 0x01, 0x67, 0x2b, 0xfe, 0xd7, 0xab, 0x76,
0xca, 0x82, 0xc9, 0x7d, 0xfa, 0x59, 0x47, 0xf0, 0xad, 0xd4, 0xa2, 0xaf, 0x9c, 0xa4, 0x72, 0xc0,
0xb7, 0xfd, 0x93, 0x26, 0x36, 0x3f, 0xf7, 0xcc, 0x34, 0xa5, 0xe5, 0xf1, 0x71, 0xd8, 0x31, 0x15,
0x04, 0xc7, 0x23, 0xc3, 0x18, 0x96, 0x05, 0x9a, 0x07, 0x12, 0x80, 0xe2, 0xeb, 0x27, 0xb2, 0x75,
0x09, 0x83, 0x2c, 0x1a, 0x1b, 0x6e, 0x5a, 0xa0, 0x52, 0x3b, 0xd6, 0xb3, 0x29, 0xe3, 0x2f, 0x84,
0x53, 0xd1, 0x00, 0xed, 0x20, 0xfc, 0xb1, 0x5b, 0x6a, 0xcb, 0xbe, 0x39, 0x4a, 0x4c, 0x58, 0xcf,
0xd0, 0xef, 0xaa, 0xfb, 0x43, 0x4d, 0x33, 0x85, 0x45, 0xf9, 0x02, 0x7f, 0x50, 0x3c, 0x9f, 0xa8,
0x51, 0xa3, 0x40, 0x8f, 0x92, 0x9d, 0x38, 0xf5, 0xbc, 0xb6, 0xda, 0x21, 0x10, 0xff, 0xf3, 0xd2,
0xcd, 0x0c, 0x13, 0xec, 0x5f, 0x97, 0x44, 0x17, 0xc4, 0xa7, 0x7e, 0x3d, 0x64, 0x5d, 0x19, 0x73,
0x60, 0x81, 0x4f, 0xdc, 0x22, 0x2a, 0x90, 0x88, 0x46, 0xee, 0xb8, 0x14, 0xde, 0x5e, 0x0b, 0xdb,
0xe0, 0x32, 0x3a, 0x0a, 0x49, 0x06, 0x24, 0x5c, 0xc2, 0xd3, 0xac, 0x62, 0x91, 0x95, 0xe4, 0x79,
0xe7, 0xc8, 0x37, 0x6d, 0x8d, 0xd5, 0x4e, 0xa9, 0x6c, 0x56, 0xf4, 0xea, 0x65, 0x7a, 0xae, 0x08,
0xba, 0x78, 0x25, 0x2e, 0x1c, 0xa6, 0xb4, 0xc6, 0xe8, 0xdd, 0x74, 0x1f, 0x4b, 0xbd, 0x8b, 0x8a,
0x70, 0x3e, 0xb5, 0x66, 0x48, 0x03, 0xf6, 0x0e, 0x61, 0x35, 0x57, 0xb9, 0x86, 0xc1, 0x1d, 0x9e,
0xe1, 0xf8, 0x98, 0x11, 0x69, 0xd9, 0x8e, 0x94, 0x9b, 0x1e, 0x87, 0xe9, 0xce, 0x55, 0x28, 0xdf,
0x8c, 0xa1, 0x89, 0x0d, 0xbf, 0xe6, 0x42, 0x68, 0x41, 0x99, 0x2d, 0x0f, 0xb0, 0x54, 0xbb, 0x16 }