SimpleLink API Reference Manual
1.11
|
Go to the source code of this file.
Data Structures | |
struct | _bsd_accept_return_t |
struct | _bsd_read_return_t |
struct | _bsd_select_return_t |
struct | _bsd_getsockopt_return_t |
struct | _bsd_gethostbyname_return_t |
Macros | |
#define | M_BSD_RESP_PARAMS_OFFSET(hci_event_hdr) ((char *)(hci_event_hdr) + HCI_EVENT_HEADER_SIZE) |
#define | SOCKET_STATUS_ACTIVE 0 |
#define | SOCKET_STATUS_INACTIVE 1 |
#define | SOCKET_STATUS_INIT_VAL 0xFFFF |
#define | M_IS_VALID_SD(sd) ((0 <= (sd)) && ((sd) <= 7)) |
#define | M_IS_VALID_STATUS(status) (((status) == SOCKET_STATUS_ACTIVE)||((status) == SOCKET_STATUS_INACTIVE)) |
#define | BSD_RECV_FROM_FROMLEN_OFFSET (4) |
#define | BSD_RECV_FROM_FROM_OFFSET (16) |
Typedefs | |
typedef struct _bsd_accept_return_t | tBsdReturnParams |
typedef struct _bsd_read_return_t | tBsdReadReturnParams |
typedef struct _bsd_select_return_t | tBsdSelectRecvParams |
typedef struct _bsd_getsockopt_return_t | tBsdGetSockOptReturnParams |
typedef struct _bsd_gethostbyname_return_t | tBsdGethostbynameParams |
Functions | |
unsigned char * | hci_event_handler (void *pRetParams, unsigned char *from, unsigned char *fromlen) |
Parse the incoming events packets and issues corresponding event handler from global array of handlers pointers. | |
long | hci_unsol_event_handler (char *event_hdr) |
Handle unsolicited events. | |
long | hci_unsolicited_event_handler (void) |
Parse the incoming unsolicited event packets and issues corresponding event handler. | |
void | set_socket_active_status (long Sd, long Status) |
long | get_socket_active_status (long Sd) |
Variables | |
unsigned long | socket_active_status |
#define M_BSD_RESP_PARAMS_OFFSET | ( | hci_event_hdr | ) | ((char *)(hci_event_hdr) + HCI_EVENT_HEADER_SIZE) |
Definition at line 100 of file evnt_handler.h.
#define SOCKET_STATUS_ACTIVE 0 |
Definition at line 102 of file evnt_handler.h.
#define SOCKET_STATUS_INACTIVE 1 |
Definition at line 103 of file evnt_handler.h.
#define SOCKET_STATUS_INIT_VAL 0xFFFF |
Definition at line 106 of file evnt_handler.h.
#define M_IS_VALID_SD | ( | sd | ) | ((0 <= (sd)) && ((sd) <= 7)) |
Definition at line 107 of file evnt_handler.h.
#define M_IS_VALID_STATUS | ( | status | ) | (((status) == SOCKET_STATUS_ACTIVE)||((status) == SOCKET_STATUS_INACTIVE)) |
Definition at line 108 of file evnt_handler.h.
#define BSD_RECV_FROM_FROMLEN_OFFSET (4) |
Definition at line 131 of file evnt_handler.h.
#define BSD_RECV_FROM_FROM_OFFSET (16) |
Definition at line 132 of file evnt_handler.h.
typedef struct _bsd_accept_return_t tBsdReturnParams |
typedef struct _bsd_read_return_t tBsdReadReturnParams |
typedef struct _bsd_select_return_t tBsdSelectRecvParams |
typedef struct _bsd_getsockopt_return_t tBsdGetSockOptReturnParams |
typedef struct _bsd_gethostbyname_return_t tBsdGethostbynameParams |
unsigned char* hci_event_handler | ( | void * | pRetParams, |
unsigned char * | from, | ||
unsigned char * | fromlen | ||
) |
Parse the incoming events packets and issues corresponding event handler from global array of handlers pointers.
hci_event_handler
pRetParams | incoming data buffer |
from | from information (in case of data received) |
fromlen | from information length (in case of data received) |
long hci_unsol_event_handler | ( | char * | event_hdr | ) |
Handle unsolicited events.
hci_unsol_event_handler
event_hdr | event header |
long hci_unsolicited_event_handler | ( | void | ) |
Parse the incoming unsolicited event packets and issues corresponding event handler.
hci_unsolicited_event_handler
None |
void set_socket_active_status | ( | long | Sd, |
long | Status | ||
) |
long get_socket_active_status | ( | long | Sd | ) |
unsigned long socket_active_status |