SimpleLink API Reference Manual  1.11
 All Data Structures Files Functions Variables Typedefs Macros Groups
nvmem.h File Reference
#include "cc3000_common.h"

Go to the source code of this file.

Macros

#define NVMEM_NVS_FILEID   (0)
 
#define NVMEM_NVS_SHADOW_FILEID   (1)
 
#define NVMEM_WLAN_CONFIG_FILEID   (2)
 
#define NVMEM_WLAN_CONFIG_SHADOW_FILEID   (3)
 
#define NVMEM_WLAN_DRIVER_SP_FILEID   (4)
 
#define NVMEM_WLAN_FW_SP_FILEID   (5)
 
#define NVMEM_MAC_FILEID   (6)
 
#define NVMEM_FRONTEND_VARS_FILEID   (7)
 
#define NVMEM_IP_CONFIG_FILEID   (8)
 
#define NVMEM_IP_CONFIG_SHADOW_FILEID   (9)
 
#define NVMEM_BOOTLOADER_SP_FILEID   (10)
 
#define NVMEM_RM_FILEID   (11)
 
#define NVMEM_AES128_KEY_FILEID   (12)
 
#define NVMEM_SHARED_MEM_FILEID   (13)
 
#define NVMEM_MAX_ENTRY   (16)
 

Functions

signed long nvmem_read (unsigned long file_id, unsigned long length, unsigned long offset, unsigned char *buff)
 Reads data from the file referred by the ulFileId parameter. Reads data from file ulOffset till length. Err if the file can't be used, is invalid, or if the read is out of bounds.
 
signed long nvmem_write (unsigned long ulFileId, unsigned long ulLength, unsigned long ulEntryOffset, unsigned char *buff)
 Write data to nvmem. writes data to file referred by the ulFileId parameter. Writes data to file ulOffset till ulLength.The file id will be marked invalid till the write is done. The file entry doesn't need to be valid - only allocated.
 
unsigned char nvmem_set_mac_address (unsigned char *mac)
 Write MAC address to EEPROM. mac address as appears over the air (OUI first)
 
unsigned char nvmem_get_mac_address (unsigned char *mac)
 Read MAC address from EEPROM. mac address as appears over the air (OUI first)
 
unsigned char nvmem_write_patch (unsigned long ulFileId, unsigned long spLength, const unsigned char *spData)
 program a patch to a specific file ID. The SP data is assumed to be organized in 2-dimensional. Each line is SP_PORTION_SIZE bytes long. Actual programming is applied in SP_PORTION_SIZE bytes portions.
 
unsigned char nvmem_read_sp_version (unsigned char *patchVer)
 Read patch version. read package version (WiFi FW patch, driver-supplicant-NS patch, bootloader patch)
 
signed long nvmem_create_entry (unsigned long file_id, unsigned long newlen)
 Create new file entry and allocate space on the NVMEM. Applies only to user files. Modify the size of file. If the entry is unallocated - allocate it to size ulNewLen (marked invalid). If it is allocated then deallocate it first. To just mark the file as invalid without resizing - set ulNewLen=0.