Data Fields | |
SlrxFilterID_t | ParentFilterID |
SlrxFilterCounterId_t | Trigger |
SlrxFilterTriggerConnectionStates_t | TriggerArgConnectionState |
SlrxFilterTriggerRoles_t | TriggerArgRoleStatus |
SlrxFilterDBTriggerArg_t | TriggerArg |
SlrxTriggerCompareFunction_t | TriggerCompareFunction |
_u8 | Padding [3] |
Definition at line 624 of file wlan_rx_filters.h.
_u8 Padding[3] |
Definition at line 652 of file wlan_rx_filters.h.
SlrxFilterID_t ParentFilterID |
The parent filter ID, this is the way to build filter tree.
Definition at line 630 of file wlan_rx_filters.h.
SlrxFilterCounterId_t Trigger |
Definition at line 633 of file wlan_rx_filters.h.
SlrxFilterDBTriggerArg_t TriggerArg |
Definition at line 642 of file wlan_rx_filters.h.
SlrxFilterTriggerConnectionStates_t TriggerArgConnectionState |
Definition at line 636 of file wlan_rx_filters.h.
SlrxFilterTriggerRoles_t TriggerArgRoleStatus |
Definition at line 639 of file wlan_rx_filters.h.
SlrxTriggerCompareFunction_t TriggerCompareFunction |
The compare function which will be operate for each bit that is turned on in the ::SlrxFilterTrigger_t.Trigger field, for example , in case the second bit in the Trigger function is on the second function in the list will be executed.
Definition at line 648 of file wlan_rx_filters.h.