Data Fields | |
SlrxFilterActionType_t | ActionType |
SlrxFilterActionArg_t | ActionArg [SL_RX_FILTER_NUM_OF_BYTES_FOR_ACTIONS_ARGS] |
_u8 | Padding [2] |
Definition at line 705 of file wlan_rx_filters.h.
SlrxFilterActionArg_t ActionArg[SL_RX_FILTER_NUM_OF_BYTES_FOR_ACTIONS_ARGS] |
location 0 - The counter to increase In case the action is of type "increase" the arg will contain the counter number, The counter number values are as in ::SlrxFilterCounterId_t.
location 1 - The template arg.
location 2 - The event arg.
Definition at line 720 of file wlan_rx_filters.h.
SlrxFilterActionType_t ActionType |
Definition at line 709 of file wlan_rx_filters.h.
_u8 Padding[2] |
Definition at line 724 of file wlan_rx_filters.h.