CC3200 Peripheral Driver Library User's Guide  1.2.0
GPIO_General_Purpose_InputOutput_api

Functions

void GPIODirModeSet (unsigned long ulPort, unsigned char ucPins, unsigned long ulPinIO)
 
unsigned long GPIODirModeGet (unsigned long ulPort, unsigned char ucPin)
 
void GPIOIntTypeSet (unsigned long ulPort, unsigned char ucPins, unsigned long ulIntType)
 
unsigned long GPIOIntTypeGet (unsigned long ulPort, unsigned char ucPin)
 
void GPIOIntEnable (unsigned long ulPort, unsigned long ulIntFlags)
 
void GPIOIntDisable (unsigned long ulPort, unsigned long ulIntFlags)
 
long GPIOIntStatus (unsigned long ulPort, tBoolean bMasked)
 
void GPIOIntClear (unsigned long ulPort, unsigned long ulIntFlags)
 
void GPIOIntRegister (unsigned long ulPort, void(*pfnIntHandler)(void))
 
void GPIOIntUnregister (unsigned long ulPort)
 
long GPIOPinRead (unsigned long ulPort, unsigned char ucPins)
 
void GPIOPinWrite (unsigned long ulPort, unsigned char ucPins, unsigned char ucVal)
 
void GPIODMATriggerEnable (unsigned long ulPort)
 
void GPIODMATriggerDisable (unsigned long ulPort)
 

Detailed Description

Function Documentation

unsigned long GPIODirModeGet ( unsigned long  ulPort,
unsigned char  ucPin 
)

Gets the direction and mode of a pin.

Parameters
ulPortis the base address of the GPIO port.
ucPinis the pin number.

This function gets the direction and control mode for a specified pin on the selected GPIO port. The pin can be configured as either an input or output under software control, or it can be under hardware control. The type of control and direction are returned as an enumerated data type.

Returns
Returns one of the enumerated data types described for GPIODirModeSet().
void GPIODirModeSet ( unsigned long  ulPort,
unsigned char  ucPins,
unsigned long  ulPinIO 
)

Sets the direction and mode of the specified pin(s).

Parameters
ulPortis the base address of the GPIO port
ucPinsis the bit-packed representation of the pin(s).
ulPinIOis the pin direction and/or mode.

This function will set the specified pin(s) on the selected GPIO port as either an input or output under software control, or it will set the pin to be under hardware control.

The parameter ulPinIO is an enumerated data type that can be one of the following values:

  • GPIO_DIR_MODE_IN
  • GPIO_DIR_MODE_OUT

where GPIO_DIR_MODE_IN specifies that the pin will be programmed as a software controlled input, GPIO_DIR_MODE_OUT specifies that the pin will be programmed as a software controlled output.

The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.

Note
GPIOPadConfigSet() must also be used to configure the corresponding pad(s) in order for them to propagate the signal to/from the GPIO.
Returns
None.
void GPIODMATriggerDisable ( unsigned long  ulPort)

Disables a GPIO port as a trigger to start a DMA transaction.

Parameters
ulPortis the base address of the GPIO port.

This function disables a GPIO port to be used as a trigger to start a uDMA transaction. This function can be used to disable this feature if it was enabled via a call to GPIODMATriggerEnable().

Returns
None.
void GPIODMATriggerEnable ( unsigned long  ulPort)

Enables a GPIO port as a trigger to start a DMA transaction.

Parameters
ulPortis the base address of the GPIO port.

This function enables a GPIO port to be used as a trigger to start a uDMA transaction. The GPIO pin will still generate interrupts if the interrupt is enabled for the selected pin.

Returns
None.
void GPIOIntClear ( unsigned long  ulPort,
unsigned long  ulIntFlags 
)

Clears the interrupt for the specified pin(s).

Parameters
ulPortis the base address of the GPIO port.
ulIntFlagsis a bit mask of the interrupt sources to be cleared.

Clears the interrupt for the specified pin(s).

The ulIntFlags parameter has the same definition as the ulIntFlags parameter to GPIOIntEnable().

Returns
None.
void GPIOIntDisable ( unsigned long  ulPort,
unsigned long  ulIntFlags 
)

Disables the specified GPIO interrupts.

Parameters
ulPortis the base address of the GPIO port.
ulIntFlagsis the bit mask of the interrupt sources to disable.

This function disables the indicated GPIO interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

The ulIntFlags parameter is the logical OR of any of the following:

  • GPIO_INT_DMA - interrupt due to GPIO triggered DMA Done
  • GPIO_INT_PIN_0 - interrupt due to activity on Pin 0.
  • GPIO_INT_PIN_1 - interrupt due to activity on Pin 1.
  • GPIO_INT_PIN_2 - interrupt due to activity on Pin 2.
  • GPIO_INT_PIN_3 - interrupt due to activity on Pin 3.
  • GPIO_INT_PIN_4 - interrupt due to activity on Pin 4.
  • GPIO_INT_PIN_5 - interrupt due to activity on Pin 5.
  • GPIO_INT_PIN_6 - interrupt due to activity on Pin 6.
  • GPIO_INT_PIN_7 - interrupt due to activity on Pin 7.
Returns
None.
void GPIOIntEnable ( unsigned long  ulPort,
unsigned long  ulIntFlags 
)

Enables the specified GPIO interrupts.

Parameters
ulPortis the base address of the GPIO port.
ulIntFlagsis the bit mask of the interrupt sources to enable.

This function enables the indicated GPIO interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

The ulIntFlags parameter is the logical OR of any of the following:

  • GPIO_INT_DMA - interrupt due to GPIO triggered DMA Done
  • GPIO_INT_PIN_0 - interrupt due to activity on Pin 0.
  • GPIO_INT_PIN_1 - interrupt due to activity on Pin 1.
  • GPIO_INT_PIN_2 - interrupt due to activity on Pin 2.
  • GPIO_INT_PIN_3 - interrupt due to activity on Pin 3.
  • GPIO_INT_PIN_4 - interrupt due to activity on Pin 4.
  • GPIO_INT_PIN_5 - interrupt due to activity on Pin 5.
  • GPIO_INT_PIN_6 - interrupt due to activity on Pin 6.
  • GPIO_INT_PIN_7 - interrupt due to activity on Pin 7.
Returns
None.
void GPIOIntRegister ( unsigned long  ulPort,
void(*)(void)  pfnIntHandler 
)

Registers an interrupt handler for a GPIO port.

Parameters
ulPortis the base address of the GPIO port.
pfnIntHandleris a pointer to the GPIO port interrupt handling function.

This function will ensure that the interrupt handler specified by pfnIntHandler is called when an interrupt is detected from the selected GPIO port. This function will also enable the corresponding GPIO interrupt in the interrupt controller; individual pin interrupts and interrupt sources must be enabled with GPIOIntEnable().

See also
IntRegister() for important information about registering interrupt handlers.
Returns
None.
long GPIOIntStatus ( unsigned long  ulPort,
tBoolean  bMasked 
)

Gets interrupt status for the specified GPIO port.

Parameters
ulPortis the base address of the GPIO port.
bMaskedspecifies whether masked or raw interrupt status is returned.

If bMasked is set as true, then the masked interrupt status is returned; otherwise, the raw interrupt status will be returned.

Returns
Returns the current interrupt status, enumerated as a bit field of values described in GPIOIntEnable().
unsigned long GPIOIntTypeGet ( unsigned long  ulPort,
unsigned char  ucPin 
)

Gets the interrupt type for a pin.

Parameters
ulPortis the base address of the GPIO port.
ucPinis the pin number.

This function gets the interrupt type for a specified pin on the selected GPIO port. The pin can be configured as a falling edge, rising edge, or both edge detected interrupt, or it can be configured as a low level or high level detected interrupt. The type of interrupt detection mechanism is returned as an enumerated data type.

Returns
Returns one of the enumerated data types described for GPIOIntTypeSet().
void GPIOIntTypeSet ( unsigned long  ulPort,
unsigned char  ucPins,
unsigned long  ulIntType 
)

Sets the interrupt type for the specified pin(s).

Parameters
ulPortis the base address of the GPIO port.
ucPinsis the bit-packed representation of the pin(s).
ulIntTypespecifies the type of interrupt trigger mechanism.

This function sets up the various interrupt trigger mechanisms for the specified pin(s) on the selected GPIO port.

The parameter ulIntType is an enumerated data type that can be one of the following values:

  • GPIO_FALLING_EDGE
  • GPIO_RISING_EDGE
  • GPIO_BOTH_EDGES
  • GPIO_LOW_LEVEL
  • GPIO_HIGH_LEVEL

The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.

Note
In order to avoid any spurious interrupts, the user must ensure that the GPIO inputs remain stable for the duration of this function.
Returns
None.
void GPIOIntUnregister ( unsigned long  ulPort)

Removes an interrupt handler for a GPIO port.

Parameters
ulPortis the base address of the GPIO port.

This function will unregister the interrupt handler for the specified GPIO port. This function will also disable the corresponding GPIO port interrupt in the interrupt controller; individual GPIO interrupts and interrupt sources must be disabled with GPIOIntDisable().

See also
IntRegister() for important information about registering interrupt handlers.
Returns
None.
long GPIOPinRead ( unsigned long  ulPort,
unsigned char  ucPins 
)

Reads the values present of the specified pin(s).

Parameters
ulPortis the base address of the GPIO port.
ucPinsis the bit-packed representation of the pin(s).

The values at the specified pin(s) are read, as specified by ucPins. Values are returned for both input and output pin(s), and the value for pin(s) that are not specified by ucPins are set to 0.

The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.

Returns
Returns a bit-packed byte providing the state of the specified pin, where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on. Any bit that is not specified by ucPins is returned as a 0. Bits 31:8 should be ignored.
void GPIOPinWrite ( unsigned long  ulPort,
unsigned char  ucPins,
unsigned char  ucVal 
)

Writes a value to the specified pin(s).

Parameters
ulPortis the base address of the GPIO port.
ucPinsis the bit-packed representation of the pin(s).
ucValis the value to write to the pin(s).

Writes the corresponding bit values to the output pin(s) specified by ucPins. Writing to a pin configured as an input pin has no effect.

The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.

Returns
None.