SimpleLink CC3100/CC3200 Host Driver
Version 1.0.1.6
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_u8 | IntRepresentation |
Definition at line 249 of file wlan_rx_filters.h.
_u8 IntRepresentation |
The filter argument can be set as binary argument or ASCII arguments. When the bit is on the argument are binary.
When the bit is on it means the the node is enabled .
Definition at line 275 of file wlan_rx_filters.h.