SimpleLink CC3100/CC3200 Host Driver  Version 1.0.1.6
Simplifies the implementation of Internet connectivity
SlrxFilterTrigger_t Struct Reference

Data Fields

SlrxFilterID_t ParentFilterID
 
SlrxFilterCounterId_t Trigger
 
SlrxFilterTriggerConnectionStates_t TriggerArgConnectionState
 
SlrxFilterTriggerRoles_t TriggerArgRoleStatus
 
SlrxFilterDBTriggerArg_t TriggerArg
 
SlrxTriggerCompareFunction_t TriggerCompareFunction
 
_u8 Padding [3]
 

Detailed Description

Definition at line 624 of file wlan_rx_filters.h.

Field Documentation

_u8 Padding[3]

Definition at line 652 of file wlan_rx_filters.h.

SlrxFilterID_t ParentFilterID

The parent filter ID, this is the way to build filter tree.

Definition at line 630 of file wlan_rx_filters.h.

SlrxFilterCounterId_t Trigger

Definition at line 633 of file wlan_rx_filters.h.

SlrxFilterDBTriggerArg_t TriggerArg

Definition at line 642 of file wlan_rx_filters.h.

SlrxFilterTriggerConnectionStates_t TriggerArgConnectionState

Definition at line 636 of file wlan_rx_filters.h.

SlrxFilterTriggerRoles_t TriggerArgRoleStatus

Definition at line 639 of file wlan_rx_filters.h.

SlrxTriggerCompareFunction_t TriggerCompareFunction

The compare function which will be operate for each bit that is turned on in the ::SlrxFilterTrigger_t.Trigger field, for example , in case the second bit in the Trigger function is on the second function in the list will be executed.

Definition at line 648 of file wlan_rx_filters.h.


The documentation for this struct was generated from the following file: