SimpleLink CC3100/CC3200 Host Driver  Version 1.0.1.6
Simplifies the implementation of Internet connectivity
_WlanRxFilterOperationCommandBuff_t Struct Reference

#include <wlan_rx_filters.h>

Data Fields

SlrxFilterIdMask_t FilterIdMask
 
_u8 Padding [4]
 

Detailed Description

The structure is used for the interface HOST NWP.
The supported operation :
::ENABLE_DISABLE_RX_FILTER,
::REMOVE_RX_FILTER,

Definition at line 737 of file wlan_rx_filters.h.

Field Documentation

SlrxFilterIdMask_t FilterIdMask

Definition at line 740 of file wlan_rx_filters.h.

_u8 Padding[4]

Definition at line 742 of file wlan_rx_filters.h.


The documentation for this struct was generated from the following file: