SimpleLink CC3120/CC3220 Host Driver
Version 2.0.1.15
Simplifies the implementation of Internet connectivity
|
The SimpleLink driver could run on two kind of platforms:
CC32XX SimpleLink Host Driver is ported on both Non-Os and Multi Threaded OS enviroment. The Host driver is made OS independent by implementing an OS Abstraction layer. Reference implementation for OS Abstraction is available for FreeRTOS and TI-RTOS.
If you choose to work in multi-threaded environment under different operating system you will have to provide some basic adaptation routines to allow the driver to protect access to resources for different threads (locking object) and to allow synchronization between threads (sync objects). In additional the driver support running without dedicated thread allocated solely to the SimpleLink driver. If you choose to work in this mode, you should also supply a spawn method that will enable to run function on a temporary context.
porting ACTION: