#include <SDHostCC32XX.h>
§ clkRate
uint_fast32_t SDHostCC32XX_HWAttrsV1::clkRate |
§ intPriority
int_fast32_t SDHostCC32XX_HWAttrsV1::intPriority |
Internal SDHost ISR command/transfer priorty
§ baseAddr
uint_fast32_t SDHostCC32XX_HWAttrsV1::baseAddr |
SDHost Peripheral base address
§ rxChIdx
unsigned long SDHostCC32XX_HWAttrsV1::rxChIdx |
uDMA controlTable receive channel index
§ txChIdx
unsigned long SDHostCC32XX_HWAttrsV1::txChIdx |
uDMA controlTable transmit channel index
§ dataPin
uint32_t SDHostCC32XX_HWAttrsV1::dataPin |
§ cmdPin
uint32_t SDHostCC32XX_HWAttrsV1::cmdPin |
§ clkPin
uint32_t SDHostCC32XX_HWAttrsV1::clkPin |
The documentation for this struct was generated from the following file: