SimpleLink CC32xx OTA Library
Simplifies the implementation of Internet connectivity
OTA

Functions

int16_t OTA_init (OTA_runningMode runningMode, OTA_memBlock *pMemBlock, OTA_eventHandler eventHandler)
 Initialize the OTA application. More...
 
int16_t OTA_run ()
 Run the OTA App state machine. More...
 
int16_t OTA_set (OTA_option option, int32_t optionLen, uint8_t *pOptionVal, int32_t flags)
 Set OTA command/parameter. More...
 
int16_t OTA_get (OTA_option option, int32_t *pOptionLen, uint8_t *pOptionVal)
 Get the current OTA status. More...
 

Variables

uint8_t Buff [OTA_BLOCK_SIZE]
 
uint32_t IpAddress
 
uint32_t SecuredConnection
 
uint8_t ServerName [MAX_SERVER_NAME]
 
uint8_t VendorToken [MAX_VENDOR_TOKEN_SIZE]
 
uint8_t CurrentVersion [VERSION_STR_SIZE+1]
 
uint8_t NewVersion [VERSION_STR_SIZE+1]
 

Detailed Description

Function Documentation

§ OTA_get()

int16_t OTA_get ( OTA_option  option,
int32_t *  pOptionLen,
uint8_t *  pOptionVal 
)

Get the current OTA status.

Parameters
[in]pOtaLibOTA control block pointer
[in]OptionSelects the option
[in]OptionLenoption structure length
[in]pOptionValpointer to the option structure

This function gets the current OTA of active or Idle. The parameter option, could be one of the following:

EXTLIB_OTA_GET_OPT_IS_ACTIVE - Check if OTA process is active or idle
EXTLIB_OTA_GET_OPT_VERSIONS - return the current OTA version and the new update version for the user to compare
EXTLIB_OTA_GET_OPT_IS_PENDING_COMMIT - Check if the new image is in the state BUNDLE_STATE_WAITING_FOR_COMMIT
Value at pOptionVal will be set to 1 if OTA process is active, 0 if Idle

Returns
Return 0 on success, -1 otherwise.
See also
Note
Warning
Example:
For example: check if pending commit
int32_t isPendingCommit;
int32_t isPendingCommit_len;
int32_t Status;
Status = Ota_get(EXTLIB_OTA_GET_OPT_IS_PENDING_COMMIT, &isPendingCommit_len, (uint8_t *)&isPendingCommit);

Definition at line 176 of file OtaLib.c.

177 {
178  Ota_optVersionsInfo *pVersionsInfo;
179  int16_t Status = OTA_STATUS_OK;
180 
181  switch (option)
182  {
183  case EXTLIB_OTA_GET_OPT_IS_ACTIVE:
184  *(int32_t *)pOptionVal = (pOtaLib->State != OTA_STATE_IDLE);
185  *pOptionLen = sizeof(int32_t);
186  break;
187 
188  case EXTLIB_OTA_GET_OPT_VERSIONS:
189 
190  pVersionsInfo = (Ota_optVersionsInfo *)pOptionVal;
191  /* get the current version from ota.dat file */
192  OtaArchive_getCurrentVersion(pVersionsInfo->CurrentVersion);
193  /* extract the new version from OtaFileName if exists */
194  if(pOtaLib->pOtaFileName == NULL)
195  {
196  /* can be if the OTA not in the right state and still didn't read the file name */
197  /* OTA file not exists (no upadte or state before reading the ota new update */
198  memset(pVersionsInfo->NewVersion, '0', VERSION_STR_SIZE);
199  }
200  else
201  {
202  uint8_t *pVersionFileName = _ExtractFileVersion(pOtaLib->pOtaFileName, MAX_CDN_FILE_NAME_SIZE);
203  /* extract version from file */
204  memcpy(pVersionsInfo->NewVersion, pVersionFileName, VERSION_STR_SIZE);
205  }
206  pVersionsInfo->NewVersion[VERSION_STR_SIZE] = 0; /* null terminated string */
207  break;
208 
209  case EXTLIB_OTA_GET_OPT_IS_PENDING_COMMIT:
210 
211  *(int32_t *)pOptionVal = OtaArchive_getPendingCommit();
212  break;
213 
214  default:
215  _SlOtaLibTrace(("OTA_get: option %ld is not implemented\r\n", option));
216  Status = OTA_OPT_ERROR_OPTION_CODE;
217  }
218 
219  return Status;
220 }

§ OTA_init()

int16_t OTA_init ( OTA_runningMode  runningMode,
OTA_memBlock pMemBlock,
OTA_eventHandler  eventHandler 
)

Initialize the OTA application.

Parameters
[in]runningModeSupported only OTA_RUN_NON_BLOCKING
[in]pMemBlockIs the OTA library control block allocated by the application
[in]eventHandlerCallback to the app, currently not supported, need to be NULL

This function initializes the OTA application and modules. The size of the control block parameter should be enough for OTA init (currently 7800 bytes) otherwize the init will failed

Returns
Return zero ot -ve otherwise.

-OTA_INIT_ERROR - when the size of the OTA control block OtaCB_t is not enough for the OTA lib

See also
Warning
Example:
For example: To initialize OTA from host invoke
OTA_memBlock otaMemBlock;
int16_t Status;
Status = OTA_init(OTA_RUN_NON_BLOCKING, &otaMemBlock, NULL);

Definition at line 45 of file OtaLib.c.

46 {
47  _SlOtaLibTrace(("OTA_init: sizeof CdnClient=%d, sizeof OtaArchive=%d\r\n", sizeof(pOtaLib->CdnClient), sizeof(pOtaLib->OtaArchive)));
48  _SlOtaLibTrace(("OTA_init: sizeof OtaLib_t=%d, sizeof OTA_memBlock=%d\r\n", sizeof(OtaLib_t), sizeof(OTA_memBlock)));
49  if (sizeof(OtaLib_t) > sizeof(OTA_memBlock))
50  {
51  _SlOtaLibTrace(("OTA_init: ERROR buffer size OtaLib_t=%d < OTA_memBlock=%d\r\n", sizeof(OtaLib_t), sizeof(OTA_memBlock)));
52  return OTA_INIT_ERROR;
53  }
54  pOtaLib = (OtaLib_t *)pMemBlock;
55 
56  memset(pOtaLib, 0, sizeof(OtaLib_t));
57  pOtaLib->State = OTA_STATE_IDLE;
58 
59  _SlOtaLibTrace(("OTA_init: OTA lib version = %s\r\n", OTA_LIB_VERSION));
60 
61  CdnClient_Init(&pOtaLib->CdnClient, pOtaLib->NetBuf);
62  OtaArchive_init(&pOtaLib->OtaArchive);
63 
64  /* init statistics */
65  return OTA_STATUS_OK;
66 }

§ OTA_run()

int16_t OTA_run ( )

Run the OTA App state machine.

Parameters
[in]pOtaLibPointer to OTA application pointer

Run one step from the OTA application state machine. Host should repeat calling this function and examine the return value in order to check if OTA completed or got error or just need to be continued. This pattern is useful in host with NON-OS. In host with OS, host should start OTA task and continuously calling this function till OTA completed.

Returns
Return zero or +ve bitmap number on success, -ve otherwise.

-OTA_RUN_STATUS_CONTINUE - Host should continue calling sl_OtaRun
-OTA_RUN_STATUS_CONTINUE_WARNING_... - group of OTA WARNINGS, actually those are errors but the OTA will retry the process 5 times so user should continue run the OTA
-OTA_RUN_STATUS_NO_UPDATES - No updates for now, host can retry after another period of time
-OTA_RUN_STATUS_CHECK_NEWER_VERSION - OTA found newer update version, user can accept the new version by calling sl_OtaSet with option _ ACCEPT_UPDATE , or just continue running, or do another check before continue
-OTA_RUN_STATUS_CHECK_OLDER_VERSION - OTA found older update version, user can stop the OTA by calling sl_OtaSet with option _DECLINE_UPDATE , or continue running, or do another check before continue
-OTA_RUN_STATUS_DOWNLOAD_DONE - Current OTA update completed, host should move the image to BUNDLE_STATE_TESTING by calling sl_Stop and then ro reset the MCU
-OTA_RUN_ERROR_... - group of OTA ERRORS, user should stop the OTA process -OTA_RUN_ERROR_CONSECUTIVE_OTA_ERRORS - OTA process failed 5 consecutive times -OTA_RUN_ERROR_NO_SERVER_NO_VENDOR - user didn't call sl_OtaSet with EXTLIB_OTA_OPT_VENDOR_ID and EXTLIB_OTA_OPT_SERVER_INFO before running the OTA -OTA_RUN_ERROR_SECURITY_ALERT - security alert from file system, user must stop trying downloading current OTA update -OTA_RUN_ERROR_UNEXPECTED_STATE - OTA state error, must init the OTA before continue

See also
Note
Warning
Example:
For example: Run OTA from host
Status = Ota_run();

Definition at line 249 of file OtaLib.c.

250 {
251  CdnClient_t *pCdnClient = (CdnClient_t *)&pOtaLib->CdnClient;
252  int16_t Status;
253  int16_t ProcessedBytes;
254 
255  switch (pOtaLib->State)
256  {
257  case OTA_STATE_IDLE:
258 #if OTA_SERVER_TYPE == OTA_FILE_DOWNLOAD
259  /* File Server URL must be initialized before running OTA */
260  if(pOtaLib->FileUrlBuf[0] == 0)
261  {
262  return OTA_RUN_ERROR_NO_SERVER_NO_VENDOR;
263  }
264  pOtaLib->State = OTA_STATE_CONNECT_FILE_SERVER;
265 #else
266  /* serverInfo and vendorDir must be init before running OTA */
267  if ((pOtaLib->OtaServerInfo.ServerName[0] == 0) /*|| (pOtaLib->VendorDir[0] == 0)*/)
268  {
269  return OTA_RUN_ERROR_NO_SERVER_NO_VENDOR;
270  }
271 
272  pOtaLib->State = OTA_STATE_CONNECT_SERVER;
273 #endif
274  break;
275 #if OTA_SERVER_TYPE != OTA_FILE_DOWNLOAD
276  case OTA_STATE_CONNECT_SERVER:
277  _SlOtaLibTrace(("OTA_run: call CdnClient_ConnectServer OTA server=%s\r\n", pOtaLib->OtaServerInfo.ServerName));
278  Status = CdnClient_ConnectServer(pCdnClient, &pOtaLib->OtaServerInfo);
279  if( Status < 0)
280  {
281  _SlOtaLibTrace(("OTA_run: ERROR CdnClient_ConnectServer, Status=%ld\r\n", Status));
282  Status = _OtaCheckConsecutiveErrors(pOtaLib, OTA_RUN_STATUS_CONTINUE_WARNING_FAILED_CONNECT_FILE_SERVER, BACK_TO_IDLE);
283  return Status;
284  }
285  pOtaLib->State = OTA_STATE_REQ_OTA_DIR;
286  break;
287 
288  case OTA_STATE_REQ_OTA_DIR:
289  {
290  int32_t NumDirFiles;
291  _SlOtaLibTrace(("OTA_run: CdnClient_ReqOtaDir, VendorDir=%s\r\n", pOtaLib->VendorDir));
292  NumDirFiles = CdnClient_ReqOtaDir(pCdnClient, pOtaLib->VendorDir);
293  if (NumDirFiles < 0)
294  {
295  _SlOtaLibTrace(("OTA_run: ERROR CdnClient_ReqOtaDir, Status=%d\r\n", NumDirFiles));
296  Status = _OtaCheckConsecutiveErrors(pOtaLib, OTA_RUN_STATUS_CONTINUE_WARNING_FAILED_REQ_OTA_DIR, BACK_TO_IDLE);
297  return Status;
298  }
299  if (NumDirFiles == 0)
300  {
301  _SlOtaLibTrace(("OTA_run: ERROR CdnClient_ReqOtaDir - no updates\r\n"));
302  pOtaLib->ConsecutiveOtaErrors = 0;
303  pOtaLib->State = OTA_STATE_IDLE;
304  _OtaCleanToIdle(pOtaLib);
305  return OTA_RUN_STATUS_NO_UPDATES;
306  }
307  _SlOtaLibTrace(("OTA_run: CdnClient_ReqOtaDir, NumDirFiles=%ld\r\n", NumDirFiles));
308  pOtaLib->State = OTA_STATE_CHECK_ARCHIVE_NEW_UPDATE;
309  }
310  break;
311 
312  case OTA_STATE_CHECK_ARCHIVE_NEW_UPDATE:
313  {
314  uint8_t *pVersionFileName;
315  _SlOtaLibTrace(("OTA_run: CdnClient_GetNextDirFile\r\n"));
316  pOtaLib->pOtaFileName = CdnClient_GetNextDirFile(pCdnClient, &pOtaLib->OtaFileSize);
317 
318  /* check if last file in the list, still without tar file */
319  if( pOtaLib->pOtaFileName == NULL)
320  {
321  /* tar file not found, return no updates */
322  _SlOtaLibTrace(("OTA_run: ERROR CdnClient_ReqOtaDir - tar not found, no updates\r\n"));
323  pOtaLib->ConsecutiveOtaErrors = 0;
324  pOtaLib->State = OTA_STATE_IDLE;
325  _OtaCleanToIdle(pOtaLib);
326  return OTA_RUN_STATUS_NO_UPDATES;
327  }
328 
329  _SlOtaLibTrace(("OTA_run: CdnClient_GetNextDirFile: file=%s, size=%ld\r\n", pOtaLib->pOtaFileName, pOtaLib->OtaFileSize));
330 
331  if (strstr((const char *)pOtaLib->pOtaFileName, ".tar") == NULL)
332  {
333  _SlOtaLibTrace(("OTA_run: WARNING, not a tar file, filename=%s\r\n", pOtaLib->pOtaFileName));
334  /* Stay on state, check next file version */
335  pOtaLib->State = OTA_STATE_CHECK_ARCHIVE_NEW_UPDATE;
336  return OTA_RUN_STATUS_CONTINUE;
337  }
338 
339  /* continue anyway, user app can override this decision */
340  pOtaLib->State = OTA_STATE_REQ_FILE_URL;
341 
342 
343  /* Init the Tar parser module */
344  OtaArchive_init(&pOtaLib->OtaArchive);
345 
346  /* host should check the version */
347  pVersionFileName = _ExtractFileVersion(pOtaLib->pOtaFileName, MAX_CDN_FILE_NAME_SIZE);
348  if (OtaArchive_checkVersion(&pOtaLib->OtaArchive, pVersionFileName))
349  {
350  return OTA_RUN_STATUS_CHECK_NEWER_VERSION;
351  }
352  else
353  {
354  return OTA_RUN_STATUS_CHECK_OLDER_VERSION;
355  }
356  }
357 
358  case OTA_STATE_REQ_FILE_URL:
359 
360  _SlOtaLibTrace(("OTA_run: Call CdnClient_ReqFileUrl, filename = %s\r\n", pOtaLib->pOtaFileName));
361  Status = CdnClient_ReqFileUrl(pCdnClient, pOtaLib->pOtaFileName, pOtaLib->FileUrlBuf, sizeof(pOtaLib->FileUrlBuf));
362  if( Status < 0)
363  {
364  _SlOtaLibTrace(("OTA_run: ERROR CdnClient_ReqFileUrl, Status=%d\r\n", Status));
365  Status = _OtaCheckConsecutiveErrors(pOtaLib, OTA_RUN_STATUS_CONTINUE_WARNING_FAILED_REQ_FILE_URL, BACK_TO_IDLE);
366  return Status;
367  }
368 
369  /* In this stage the CDN server can be closed */
370  CdnClient_CloseServer(&pOtaLib->CdnClient);
371 
372  pOtaLib->State = OTA_STATE_CONNECT_FILE_SERVER;
373  break;
374 #endif
375  case OTA_STATE_CONNECT_FILE_SERVER:
376 
377  _SlOtaLibTrace(("OTA_run: Call CdnClient_ConnectFileServer, url = %s\r\n", pOtaLib->FileUrlBuf));
378  Status = CdnClient_ConnectFileServer(&pOtaLib->CdnClient, pOtaLib->FileUrlBuf, pOtaLib->OtaServerInfo.SecuredConnection);
379  if( Status < 0)
380  {
381  /* stay on this state for another retry */
382  _SlOtaLibTrace(("OTA_run: ERROR CdnClient_ConnectFileServer, Status=%d\r\n", Status));
383  Status = _OtaCheckConsecutiveErrors(pOtaLib, OTA_RUN_STATUS_CONTINUE_WARNING_FAILED_CONNECT_FILE_SERVER, BACK_TO_IDLE);
384  return Status;
385  }
386  pOtaLib->State = OTA_STATE_REQ_FILE_CONTENT;
387  break;
388 
389  case OTA_STATE_REQ_FILE_CONTENT:
390 
391  _SlOtaLibTrace(("OTA_run: Call CdnClient_ReqFileContent, url = %s\r\n", pOtaLib->FileUrlBuf));
392  Status = CdnClient_ReqFileContent(&pOtaLib->CdnClient, pOtaLib->FileUrlBuf);
393  if( Status < 0)
394  {
395  _SlOtaLibTrace(("OTA_run: ERROR CdnClient_ReqFileContent, Status=%d\r\n", Status));
396  Status = _OtaCheckConsecutiveErrors(pOtaLib, OTA_RUN_STATUS_CONTINUE_WARNING_FAILED_REQ_FILE_CONTENT, BACK_TO_IDLE);
397  return Status;
398  }
399 
400  pOtaLib->State = OTA_STATE_PREPARE_DOWNLOAD;
401  break;
402 
403  case OTA_STATE_PREPARE_DOWNLOAD:
404 
405  /* prepare receive buffer */
406  pOtaLib->pRecvChunk = pOtaLib->NetBuf;
407  pOtaLib->RecvChunkOffset = 0;
408  pOtaLib->RecvChunkForceReadMode = 0;
409 
410  pOtaLib->RecvChunkSize = CdnClient_RecvSkipHdr(pCdnClient->FileSockId, pOtaLib->pRecvChunk, NET_BUF_SIZE);
411  if (0 >= pOtaLib->RecvChunkSize)
412  {
413  _SlOtaLibTrace(("OTA_run: ERROR downloading, CdnClient_RecvSkipHdr Status=%ld\r\n", pOtaLib->RecvChunkSize));
414  /* Stop the parsing of the archive file */
415  OtaArchive_abort(&pOtaLib->OtaArchive);
416  Status = _OtaCheckConsecutiveErrors(pOtaLib, OTA_RUN_STATUS_CONTINUE_WARNING_FAILED_FILE_HDR, BACK_TO_IDLE);
417  return Status;
418  }
419 
420  pOtaLib->State = OTA_STATE_DOWNLOADING;
421  break;
422 
423  case OTA_STATE_DOWNLOADING:
424 
425  /* Check if to read more chunk */
426  if ((pOtaLib->RecvChunkOffset != 0) || (pOtaLib->RecvChunkSize == 0) || pOtaLib->RecvChunkForceReadMode)
427  {
428  int16_t UnprocessedSize = pOtaLib->RecvChunkSize-pOtaLib->RecvChunkOffset;
429  int16_t Len;
430 
431  if (UnprocessedSize >= TAR_HDR_SIZE)
432  {
433  /* No need to read more, enough unprocessed bytes to decode next TAR file header */
434  memcpy(&pOtaLib->pRecvChunk[0], &pOtaLib->pRecvChunk[pOtaLib->RecvChunkOffset], UnprocessedSize);
435  Len = UnprocessedSize;
436  }
437  else
438  {
439  Len = CdnClient_RecvAppend(pCdnClient->FileSockId, pOtaLib->pRecvChunk, NET_BUF_SIZE, pOtaLib->RecvChunkSize, pOtaLib->RecvChunkOffset);
440  }
441  if (0 >= Len)
442  {
443  _SlOtaLibTrace(("OTA_run: ERROR downloading, CdnClient_RecvAppend Status=%ld\r\n", Len));
444  /* Stop the parsing of the archive file */
445  OtaArchive_abort(&pOtaLib->OtaArchive);
446  Status = _OtaCheckConsecutiveErrors(pOtaLib, OTA_RUN_STATUS_CONTINUE_WARNING_FAILED_RECV_APPEND, BACK_TO_IDLE);
447  return Status;
448  }
449  pOtaLib->RecvChunkOffset = 0;
450  pOtaLib->RecvChunkSize = Len;
451  pOtaLib->RecvChunkForceReadMode = 0;
452  }
453 
454  Status = OtaArchive_process(&pOtaLib->OtaArchive, pOtaLib->pRecvChunk, pOtaLib->RecvChunkSize, &ProcessedBytes);
455  pOtaLib->RecvChunkForceReadMode = (Status == ARCHIVE_STATUS_FORCE_READ_MORE);
456  pOtaLib->RecvChunkOffset += ProcessedBytes;
457  if( Status < 0)
458  {
459  if (Status == ARCHIVE_STATUS_ERROR_SECURITY_ALERT)
460  {
461  _SlOtaLibTrace(("OTA_run: SECURITY ALERT OtaArchive_RunParse, Status=%d\r\n", Status));
462  /* On SECURITY ALERT, stop all, no consecutive errors check */
463  pOtaLib->State = OTA_STATE_IDLE;
464  _OtaCleanToIdle(pOtaLib);
465  Status = OTA_RUN_ERROR_SECURITY_ALERT;
466  }
467  else
468  {
469  _SlOtaLibTrace(("OTA_run: ERROR OtaArchive_RunParse, Status=%d\r\n", Status));
470  Status = _OtaCheckConsecutiveErrors(pOtaLib, OTA_RUN_STATUS_CONTINUE_WARNING_FAILED_DOWNLOAD_AND_SAVE, BACK_TO_IDLE);
471  }
472  return Status;
473  }
474  else if (Status == ARCHIVE_STATUS_DOWNLOAD_DONE)
475  {
476  _SlOtaLibTrace(("OTA_run: ---- Download file completed %s\r\n", pOtaLib->pOtaFileName));
477  CdnClient_CloseFileServer(&pOtaLib->CdnClient);
478  pOtaLib->State = OTA_STATE_WAIT_CONFIRM; /* not real state, cannot go to idle, user app should reset */
479  pOtaLib->ConsecutiveOtaErrors = 0;
480 
481  return OTA_RUN_STATUS_DOWNLOAD_DONE;
482  }
483  break;
484 
485  case OTA_STATE_WAIT_CONFIRM:
486  /* not real state, cannot go to idle, user app should reset */
487  _SlOtaLibTrace(("sl_OtaRun ERROR: unexpected state %d\r\n", pOtaLib->State));
488  return OTA_RUN_STATUS_DOWNLOAD_DONE;
489 
490  default:
491  _SlOtaLibTrace(("sl_OtaRun ERROR: unexpected state %d\r\n", pOtaLib->State));
492  return OTA_RUN_ERROR_UNEXPECTED_STATE;
493 
494  }
495 
496  return OTA_RUN_STATUS_CONTINUE;
497 }

§ OTA_set()

int16_t OTA_set ( OTA_option  option,
int32_t  optionLen,
uint8_t *  pOptionVal,
int32_t  flags 
)

Set OTA command/parameter.

Parameters
[in]pOtaLibOTA control block pointer
[in]OptionSelect the option
[in]OptionLenOption structure length
[in]pOptionValpointer to the option structure

This function sets OTA command/parameter. The parameter Option can be one of the following:

EXTLIB_OTA_SET_OPT_SERVER_INFO - Set the Server information
EXTLIB_OTA_SET_OPT_VENDOR_ID - Set the Vendor DIR string
EXTLIB_OTA_SET_OPT_ACCEPT_UPDATE - Accept the new image
EXTLIB_OTA_SET_OPT_DECLINE_UPDATE - Decline the new image
EXTLIB_OTA_SET_OPT_IMAGE_COMMIT - Commit the currnet image in testing mode
EXTLIB_OTA_SET_OPT_IMAGE_ROLLBACK - decline the currnet image in testing mode and rollback to the previous image

Returns
On success, zero is returned. On error, -1 is returned
See also
Note
Warning
Example:
For example: Set OTA server info from host
Ota_optServerInfo g_otaOptServerInfo;
g_otaOptServerInfo.IpAddress = OTA_SERVER_IP_ADDRESS;
g_otaOptServerInfo.SecuredConnection = OTA_SERVER_SECURED;
strcpy((char *)g_otaOptServerInfo.ServerName, OTA_SERVER_NAME);
strcpy((char *)g_otaOptServerInfo.VendorToken, OTA_VENDOR_TOKEN);
Status = Ota_set(EXTLIB_OTA_SET_OPT_SERVER_INFO, sizeof(g_otaOptServerInfo), (uint8_t *)&g_otaOptServerInfo);
Ota_set(EXTLIB_OTA_SET_OPT_SERVER_INFO, sizeof(g_otaOptServerInfo), (uint8_t *)&g_otaOptServerInfo, 0);

Definition at line 99 of file OtaLib.c.

100 {
101  int16_t Status = OTA_STATUS_OK;
102 
103  switch (option)
104  {
105  case EXTLIB_OTA_SET_OPT_SERVER_INFO:
106  memcpy(&pOtaLib->OtaServerInfo, pOptionVal, sizeof(Ota_optServerInfo));
107  break;
108 
109  case EXTLIB_OTA_SET_OPT_FILE_SERVER_URL:
110  strcpy((char *)pOtaLib->FileUrlBuf, (char *)pOptionVal);
111  pOtaLib->OtaServerInfo.SecuredConnection = OTA_SERVER_SECURED;
112  break;
113 
114  case EXTLIB_OTA_SET_OPT_VENDOR_ID:
115  if (strlen((const char *)pOptionVal) >= MAX_VENDIR_DIR_SIZE)
116  {
117  return OTA_OPT_ERROR_VENDOR_DIR_SIZE;
118  }
119  strcpy((char *)pOtaLib->VendorDir, (const char *)pOptionVal);
120  break;
121 
122  case EXTLIB_OTA_SET_OPT_ACCEPT_UPDATE:
123  /* do nothing, the OTA is already on process and not in IDLE state */
124  break;
125 
126  case EXTLIB_OTA_SET_OPT_DECLINE_UPDATE:
127 
128  /* check if after OTA_STATE_CHECK_ARCHIVE_NEW_UPDATE state */
129  if (pOtaLib->State != OTA_STATE_REQ_FILE_URL)
130  {
131  _SlOtaLibTrace(("OTA_set: ERROR EXTLIB_OTA_SET_OPT_DECLINE_UPDATE in wrong state = %d\r\n", pOtaLib->State));
132  return OTA_OPT_ERROR_WRONG_STATE;
133  }
134 
135  /* close all connection from last OTA updates and back to IDLE */
136  pOtaLib->ConsecutiveOtaErrors = 0;
137  _OtaCleanToIdle(pOtaLib);
138  break;
139 
140  case EXTLIB_OTA_SET_OPT_IMAGE_COMMIT:
141 
142  Status = OtaArchive_commit();
143  if (Status < 0)
144  {
145  _SlOtaLibTrace(("OTA_set: ERROR OtaArchive_Commit, status=%d\r\n", Status));
146  return OTA_OPT_ERROR_COMMIT;
147  }
148 
149 
150  break;
151 
152  case EXTLIB_OTA_SET_OPT_IMAGE_ROLLBACK:
153 
154  Status = OtaArchive_rollback();
155  if (Status < 0)
156  {
157  if (Status == SL_ERROR_FS_BUNDLE_NOT_IN_CORRECT_STATE)
158  {
159  _SlOtaLibTrace(("OTA_set: ERROR OtaArchive_Rollback, status=%d - ignored SL_ERROR_FS_BUNDLE_NOT_IN_CORRECT_STATE\r\n", Status));
160  /* Ignore error calling rollback in the incorrect state */
161  return OTA_STATUS_OK;
162  }
163  _SlOtaLibTrace(("OTA_set: ERROR OtaArchive_Rollback, status=%d\r\n", Status));
164  return OTA_OPT_ERROR_ROLLBACK;
165  }
166  break;
167 
168  default:
169  _SlOtaLibTrace(("OTA_set: option %ld is not implemented\r\n", option));
170  return OTA_OPT_ERROR_OPTION_CODE;
171  }
172 
173  return Status;
174 }

Variable Documentation

§ Buff

uint8_t Buff[OTA_BLOCK_SIZE]

Definition at line 56 of file ota.h.

§ CurrentVersion

uint8_t CurrentVersion[VERSION_STR_SIZE+1]

Definition at line 83 of file ota.h.

§ IpAddress

uint32_t IpAddress

Definition at line 75 of file ota.h.

§ NewVersion

uint8_t NewVersion[VERSION_STR_SIZE+1]

Definition at line 84 of file ota.h.

§ SecuredConnection

uint32_t SecuredConnection

Definition at line 76 of file ota.h.

§ ServerName

uint8_t ServerName[MAX_SERVER_NAME]

Definition at line 77 of file ota.h.

§ VendorToken

uint8_t VendorToken[MAX_VENDOR_TOKEN_SIZE]

Definition at line 78 of file ota.h.