Data Structures | Macros | Typedefs | Variables
I2CCC32XX.h File Reference

Detailed Description

I2C driver implementation for a CC32XX I2C controller.


The I2C header file should be included in an application as follows:

Refer to I2C.h for a complete description of APIs and usage.

Supported Bit Rates

#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/I2C.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/Power.h>
Include dependency graph for I2CCC32XX.h:

Go to the source code of this file.

Data Structures

struct  I2CCC32XX_HWAttrsV1
 I2CCC32XX Hardware attributes. More...
 

Macros

#define I2CCC32XX_PIN_01_I2C_SCL   0x100
 
#define I2CCC32XX_PIN_02_I2C_SDA   0x101
 
#define I2CCC32XX_PIN_03_I2C_SCL   0x502
 
#define I2CCC32XX_PIN_04_I2C_SDA   0x503
 
#define I2CCC32XX_PIN_05_I2C_SCL   0x504
 
#define I2CCC32XX_PIN_06_I2C_SDA   0x505
 
#define I2CCC32XX_PIN_16_I2C_SCL   0x90F
 
#define I2CCC32XX_PIN_17_I2C_SDA   0x910
 

Typedefs

typedef struct I2CCC32XX_HWAttrsV1 I2CCC32XX_HWAttrsV1
 I2CCC32XX Hardware attributes. More...
 

Variables

const I2C_FxnTable I2CCC32XX_fxnTable
 

Macro Definition Documentation

§ I2CCC32XX_PIN_01_I2C_SCL

#define I2CCC32XX_PIN_01_I2C_SCL   0x100

PIN 1 is used for I2C_SCL

§ I2CCC32XX_PIN_02_I2C_SDA

#define I2CCC32XX_PIN_02_I2C_SDA   0x101

PIN 2 is used for I2C_SDA

§ I2CCC32XX_PIN_03_I2C_SCL

#define I2CCC32XX_PIN_03_I2C_SCL   0x502

PIN 3 is used for I2C_SCL

§ I2CCC32XX_PIN_04_I2C_SDA

#define I2CCC32XX_PIN_04_I2C_SDA   0x503

PIN 4 is used for I2C_SDA

§ I2CCC32XX_PIN_05_I2C_SCL

#define I2CCC32XX_PIN_05_I2C_SCL   0x504

PIN 5 is used for I2C_SCL

§ I2CCC32XX_PIN_06_I2C_SDA

#define I2CCC32XX_PIN_06_I2C_SDA   0x505

PIN 6 is used for I2C_SDA

§ I2CCC32XX_PIN_16_I2C_SCL

#define I2CCC32XX_PIN_16_I2C_SCL   0x90F

PIN 16 is used for I2C_SCL

§ I2CCC32XX_PIN_17_I2C_SDA

#define I2CCC32XX_PIN_17_I2C_SDA   0x910

PIN 17 is used for I2C_SDA

Typedef Documentation

§ I2CCC32XX_HWAttrsV1

I2CCC32XX Hardware attributes.

The baseAddr and intNum fields define the base address and interrupt number of the I2C peripheral. These values are used by driverlib APIs and therefore must be populated by driverlib macro definitions. These definitions are found in the header files:

  • inc/hw_memmap.h
  • inc/hw_ints.h

intPriority is the I2C peripheral's interrupt priority. This driver uses the ti.dpl interface instead of making OS calls directly, and the corresponding HwiP port handles the interrupt priority in an OS-specific way. For example, in the case of the TI-RTOS kernel port, the intPriority is passed unmodified to Hwi_create() provided by the ti.sysbios.family.arm.m3.Hwi module; so the documentation for the ti.sysbios.family.arm.m3.Hwi module should be referenced for a description of usage of priority.

clkPin and dataPin define the pin multiplexing to be used for the SCL and SDA pins, respectively. Macro values defined in this header file should be used for these fields.

A sample structure is shown below:

const I2CCC32XX_HWAttrsV1 i2cCC32XXHWAttrs[] = {
{
.baseAddr = I2CA0_BASE,
.intNum = INT_I2CA0,
.intPriority = (~0),
}
};

Variable Documentation

§ I2CCC32XX_fxnTable

const I2C_FxnTable I2CCC32XX_fxnTable
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale