TimerCC32XX_Object. More...
#include <TimerCC32XX.h>
Data Fields | |
HwiP_Handle | hwiHandle |
Power_NotifyObj | notifyObj |
SemaphoreP_Handle | timerSem |
Timer_CallBackFxn | callBack |
Timer_Mode | mode |
uint32_t | timer |
uint32_t | period |
uint32_t | prescaler |
bool | isRunning |
TimerCC32XX_Object.
The application must not access any member variables of this structure!
HwiP_Handle TimerCC32XX_Object_::hwiHandle |
Power_NotifyObj TimerCC32XX_Object_::notifyObj |
SemaphoreP_Handle TimerCC32XX_Object_::timerSem |
Timer_CallBackFxn TimerCC32XX_Object_::callBack |
Timer_Mode TimerCC32XX_Object_::mode |
uint32_t TimerCC32XX_Object_::timer |
uint32_t TimerCC32XX_Object_::period |
uint32_t TimerCC32XX_Object_::prescaler |
bool TimerCC32XX_Object_::isRunning |