Data Fields
SPI_Config_ Struct Reference

SPI Global configuration. More...

#include <SPI.h>

Data Fields

SPI_FxnTable const * fxnTablePtr
 
void * object
 
void const * hwAttrs
 

Detailed Description

SPI Global configuration.

The SPI_Config structure contains a set of pointers used to characterize the SPI driver implementation.

This structure needs to be defined before calling SPI_init() and it must not be changed thereafter.

See also
SPI_init()

Field Documentation

§ fxnTablePtr

SPI_FxnTable const* SPI_Config_::fxnTablePtr

Pointer to a table of driver-specific implementations of SPI APIs

§ object

void* SPI_Config_::object

Pointer to a driver specific data object

§ hwAttrs

void const* SPI_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated