Data Fields
PowerCC32XX_Wakeup Struct Reference

Specify the wakeup sources for LPDS and Shutdown. More...

#include <PowerCC32XX.h>

Data Fields

bool enableGPIOWakeupLPDS
 
bool enableGPIOWakeupShutdown
 
bool enableNetworkWakeupLPDS
 
uint32_t wakeupGPIOSourceLPDS
 The GPIO source for wakeup from LPDS. More...
 
uint32_t wakeupGPIOTypeLPDS
 The GPIO trigger type for wakeup from LPDS. More...
 
void(* wakeupGPIOFxnLPDS )(uint_least8_t argument)
 Function to be called when the configured GPIO triggers wakeup from LPDS. More...
 
uint_least8_t wakeupGPIOFxnLPDSArg
 The argument to be passed to wakeupGPIOFxnLPDS() More...
 
uint32_t wakeupGPIOSourceShutdown
 The GPIO sources for wakeup from shutdown. More...
 
uint32_t wakeupGPIOTypeShutdown
 The GPIO trigger type for wakeup from shutdown. More...
 

Detailed Description

Specify the wakeup sources for LPDS and Shutdown.

The wakeup sources for LPDS and Shutdown can be dynamically changed at runtime, via PowerCC32XX_configureWakeup(). The application should fill a structure of this type, and pass it as the parameter to PowerCC32XX_configureWakeup() to specify the new wakeup settings.

Field Documentation

§ enableGPIOWakeupLPDS

bool PowerCC32XX_Wakeup::enableGPIOWakeupLPDS

Enable GPIO as a wakeup source for LPDS

§ enableGPIOWakeupShutdown

bool PowerCC32XX_Wakeup::enableGPIOWakeupShutdown

Enable GPIO as a wakeup source for shutdown

§ enableNetworkWakeupLPDS

bool PowerCC32XX_Wakeup::enableNetworkWakeupLPDS

Enable Network activity as a wakeup source for LPDS

§ wakeupGPIOSourceLPDS

uint32_t PowerCC32XX_Wakeup::wakeupGPIOSourceLPDS

The GPIO source for wakeup from LPDS.

Only one GPIO {2,4,11,13,17,24,26} can be specified as a wake source for LPDS. The GPIO must be specified as one of the following (as defined in driverlib/prcm.h): PRCM_LPDS_GPIO2, PRCM_LPDS_GPIO4, PRCM_LPDS_GPIO11, PRCM_LPDS_GPIO13, PRCM_LPDS_GPIO17, PRCM_LPDS_GPIO24, PRCM_LPDS_GPIO26

§ wakeupGPIOTypeLPDS

uint32_t PowerCC32XX_Wakeup::wakeupGPIOTypeLPDS

The GPIO trigger type for wakeup from LPDS.

Value can be one of the following (defined in driverlib/prcm.h): PRCM_LPDS_LOW_LEVEL, PRCM_LPDS_HIGH_LEVEL, PRCM_LPDS_FALL_EDGE, PRCM_LPDS_RISE_EDGE

§ wakeupGPIOFxnLPDS

void(* PowerCC32XX_Wakeup::wakeupGPIOFxnLPDS) (uint_least8_t argument)

Function to be called when the configured GPIO triggers wakeup from LPDS.

During LPDS the internal GPIO module is powered off, and special periphery logic is used instead to detect the trigger and wake the device. No GPIO interrupt service routine will be triggered in this case (even if an ISR is configured, and used normally to detect GPIO interrupts when not in LPDS). This function can be used in lieu of a GPIO ISR, to take specific action upon LPDS wakeup.

A value of NULL indicates no GPIO wakeup function will be called.

An argument for this wakeup function can be specified via wakeupGPIOFxnLPDSArg.

Note that this wakeup function will be called as one of the last steps in Power_sleep(), after all notifications have been sent out, and after pins have been restored to their previous (non-parked) states.

§ wakeupGPIOFxnLPDSArg

uint_least8_t PowerCC32XX_Wakeup::wakeupGPIOFxnLPDSArg

The argument to be passed to wakeupGPIOFxnLPDS()

§ wakeupGPIOSourceShutdown

uint32_t PowerCC32XX_Wakeup::wakeupGPIOSourceShutdown

The GPIO sources for wakeup from shutdown.

Only one GPIO {2,4,11,13,17,24,26} can be specified as a wake source for Shutdown. The GPIO must be specified as one of the following (as defined in driverlib/prcm.h): PRCM_HIB_GPIO2, PRCM_HIB_GPIO4, PRCM_HIB_GPIO11, PRCM_HIB_GPIO13, PRCM_HIB_GPIO17, PRCM_HIB_GPIO24, PRCM_HIB_GPIO26

§ wakeupGPIOTypeShutdown

uint32_t PowerCC32XX_Wakeup::wakeupGPIOTypeShutdown

The GPIO trigger type for wakeup from shutdown.

Value can be one of the following (defined in driverlib/prcm.h): PRCM_HIB_LOW_LEVEL, PRCM_HIB_HIGH_LEVEL, PRCM_HIB_FALL_EDGE, PRCM_HIB_RISE_EDGE


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated