Data Fields
PWMTimerCC32XX_Object Struct Reference

PWMTimerCC32XX Object. More...

#include <PWMTimerCC32XX.h>

Data Fields

Power_NotifyObj postNotify
 
uint32_t duty
 
uint32_t period
 
PWM_Duty_Units dutyUnits
 
PWM_Period_Units periodUnits
 
PWM_IdleLevel idleLevel
 
bool pwmStarted
 
bool isOpen
 

Detailed Description

PWMTimerCC32XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ postNotify

Power_NotifyObj PWMTimerCC32XX_Object::postNotify

§ duty

uint32_t PWMTimerCC32XX_Object::duty

§ period

uint32_t PWMTimerCC32XX_Object::period

§ dutyUnits

PWM_Duty_Units PWMTimerCC32XX_Object::dutyUnits

§ periodUnits

PWM_Period_Units PWMTimerCC32XX_Object::periodUnits

§ idleLevel

PWM_IdleLevel PWMTimerCC32XX_Object::idleLevel

§ pwmStarted

bool PWMTimerCC32XX_Object::pwmStarted

§ isOpen

bool PWMTimerCC32XX_Object::isOpen

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated