Data Fields
I2C_Params_ Struct Reference

I2C Parameters. More...

#include <I2C.h>

Data Fields

I2C_TransferMode transferMode
 
I2C_CallbackFxn transferCallbackFxn
 
I2C_BitRate bitRate
 
void * custom
 

Detailed Description

I2C Parameters.

I2C parameters are used with the I2C_open() call. Default values for these parameters are set using I2C_Params_init().

If I2C_TransferMode is set to I2C_MODE_BLOCKING, I2C_transfer() function calls will block thread execution until the transaction has completed. In this case, the transferCallbackFxn parameter will be ignored.

If I2C_TransferMode is set to I2C_MODE_CALLBACK, I2C_transfer() will not block thread execution, but it will call the function specified by transferCallbackFxn upon transfer completion. Sequential calls to I2C_transfer() in I2C_MODE_CALLBACK will put the I2C_Transaction structures onto an internal queue that automatically starts queued transactions after the previous transaction has completed. This queuing occurs regardless of any error state from previous transactions.

I2C_BitRate specifies the I2C bus rate used for I2C communications.

See also
I2C_Params_init()

Field Documentation

§ transferMode

I2C_TransferMode I2C_Params_::transferMode

Blocking or Callback mode

§ transferCallbackFxn

I2C_CallbackFxn I2C_Params_::transferCallbackFxn

Callback function pointer

§ bitRate

I2C_BitRate I2C_Params_::bitRate

I2C bus bit rate

§ custom

void* I2C_Params_::custom

Custom argument used by driver implementation


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated