Macros | |
#define | I2SCC32XXDMA_CMD_SET_ZEROBUF_LEN (I2S_CMD_RESERVED + 0) |
#define | I2SCC32XXDMA_CMD_SET_EMPTYBUF_LEN (I2S_CMD_RESERVED + 1) |
I2S_CMD_* macros are general command codes for I2S_control(). Not all I2S driver implementations support these command codes.
I2SCC32XXDMA_CMD_* macros are command codes only defined in the I2SCC32XXDMA.h driver implementation and need to:
#define I2SCC32XXDMA_CMD_SET_ZEROBUF_LEN (I2S_CMD_RESERVED + 0) |
#define I2SCC32XXDMA_CMD_SET_EMPTYBUF_LEN (I2S_CMD_RESERVED + 1) |