Modules | Macros
Camera_control command and status codes

Modules

 Status Codes
 
 Command Codes
 

Macros

#define CAMERA_CMD_RESERVED   (32)
 
#define CAMERA_STATUS_RESERVED   (-32)
 

Detailed Description

These Camera macros are reservations for Camera.h

Macro Definition Documentation

§ CAMERA_CMD_RESERVED

#define CAMERA_CMD_RESERVED   (32)

Common Camera_control command code reservation offset. Camera driver implementations should offset command codes with CAMERA_CMD_RESERVED growing positively

Example implementation specific command codes:

#define CAMERAXYZ_CMD_COMMAND0 CAMERA_CMD_RESERVED + 0
#define CAMERAXYZ_CMD_COMMAND1 CAMERA_CMD_RESERVED + 1

§ CAMERA_STATUS_RESERVED

#define CAMERA_STATUS_RESERVED   (-32)

Common Camera_control status code reservation offset. Camera driver implementations should offset status codes with CAMERA_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define CAMERAXYZ_STATUS_ERROR0 CAMERA_STATUS_RESERVED - 0
#define CAMERAXYZ_STATUS_ERROR1 CAMERA_STATUS_RESERVED - 1
#define CAMERAXYZ_STATUS_ERROR2 CAMERA_STATUS_RESERVED - 2
Copyright 2017, Texas Instruments Incorporated