EDMA3_DRV_ChainOptions | Structure to be used to configure interrupt generation and chaining options |
EDMA3_DRV_ChBoundResources | EDMA3 Channel-Bound resources |
EDMA3_DRV_EvtQuePriority | Event queue priorities setup |
EDMA3_DRV_GblConfigParams | Init-time Configuration structure for EDMA3 controller, to provide Global SoC specific Information |
EDMA3_DRV_GblXbarToChanConfigParams | Init-time Configuration structure for EDMA3 controller, to provide Global SoC specific Information |
EDMA3_DRV_InitConfig | Used to Initialize the EDMA3 Driver Instance |
EDMA3_DRV_Instance | EDMA3 Driver Instance Configuration Structure |
EDMA3_DRV_InstanceInitConfig | Init-time Region Specific Configuration structure for EDMA3 Driver, to provide region specific Information |
EDMA3_DRV_MiscParam | Used to specify the miscellaneous options during EDMA3 Driver Initialization |
EDMA3_DRV_Object | EDMA3 Driver Object (HW Specific) Maintenance structure |
EDMA3_DRV_ParamentryRegs | EDMA3 PaRAM Set |
EDMA3_DRV_PaRAMRegs | EDMA3 Parameter RAM Set in User Configurable format |