Data Fields

XDM2_BufDesc Struct Reference
[XDM - Shared XDM Definitions]

Buffer descriptor. More...

#include <xdm.h>

Collaboration diagram for XDM2_BufDesc:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 numBufs
XDM2_SingleBufDesc descs [16]

Detailed Description

Buffer descriptor.

Remarks:
This advanced buffer uses the XDM2_SingleBufDesc, and is typically used for codecs which must reflect types of memory. For example, video codecs may need to indicate whether tiled memory is used.

Field Documentation

Number of buffers in descs array.

Remarks:
Must be less than XDM_MAX_IO_BUFFERS.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated