Data Fields

IVIDENC2_InArgs Struct Reference
[IVIDENC2 - XDM Video Encoder Interface]

Defines the input arguments for all IVIDENC2 instance process function. More...

#include <ividenc2.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 inputID
XDAS_Int32 control

Detailed Description

Defines the input arguments for all IVIDENC2 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDENC2_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Identifier to attach with the corresponding input frames to be encoded.

Remarks:
This is useful when frames require buffering (e.g. B frames), and to support buffer management.
When there is no re-ordering, IVIDENC2_OutArgs::outputID will be the same as this inputID field.
Zero (0) is not a supported inputID. This value is reserved for cases when there is no input buffer is provided.
See also:
IVIDENC2_OutArgs::outputID.

Encoder control operations

See also:
IVIDENC2_Control

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated