Data Fields

IVIDDEC2_DynamicParams Struct Reference
[IVIDDEC2 - XDM Video Decoder Interface]

This structure defines the codec parameters that can be modified after creation via control() calls. More...

#include <ividdec2.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 decodeHeader
XDAS_Int32 displayWidth
XDAS_Int32 frameSkipMode
XDAS_Int32 frameOrder
XDAS_Int32 newFrameFlag
XDAS_Int32 mbDataFlag

Detailed Description

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC2_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Decode entire access unit or only header.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
See also:
XDM_DecMode

Pitch. If set to zero, use the decoded image width. Else, use given display width in pixels.

Video frame skip features for video decoder.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
See also:
IVIDEO_FrameSkip

Video decoder output frame order.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
See also:
IVIDDEC2_DynamicParams::frameOrder
See also:
IVIDDEC2_FrameOrder

Flag to indicate that the algorithm should start a new frame.

Remarks:
Valid values are XDAS_TRUE and XDAS_FALSE.
This is useful for error recovery, for example when the end of frame cannot be detected by the codec but is known to the application.

Flag to indicate that the algorithm should generate MB Data in addition to decoding the data.

Remarks:
Valid values are XDAS_TRUE and XDAS_FALSE.
See also:
IVIDDEC2_OutArgs::mbDataBuf

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated