Data Fields

ISPHDEC_InArgs Struct Reference
[ISPHDEC - XDM Speech Decoder Interface]

Defines the input arguments for all ISPHDEC instance process function. More...

#include <isphdec.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 frameType
XDAS_Int32 inBufferSize
XDAS_Int32 bfiFlag

Detailed Description

Defines the input arguments for all ISPHDEC instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHDEC_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Input frame type.

Size of valid input data in bytes to be processed.

Bad frame indicator. BFI = 1 indicates bad frame.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated