Data Fields

IIMGENC_InArgs Struct Reference
[IIMGENC - XDM Image Encoder Interface]

Defines the input arguments for all IIMGENC instance process() function. More...

#include <iimgenc.h>

Data Fields

XDAS_Int32 size

Detailed Description

Defines the input arguments for all IIMGENC instance process() function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated