Data Fields

IIMGDEC_Status Struct Reference
[IIMGDEC - XDM Image Decoder Interface]

Defines instance status parameters (read-only). More...

#include <iimgdec.h>

Collaboration diagram for IIMGDEC_Status:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 extendedError
XDAS_Int32 outputHeight
XDAS_Int32 outputWidth
XDAS_Int32 imageWidth
XDAS_Int32 outChromaformat
XDAS_Int32 totalAU
XDAS_Int32 totalScan
XDM_AlgBufInfo bufInfo

Detailed Description

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGDEC_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.
See also:
XDM_ErrorBit

Output height.

Output width. Padding should be taken care of by the decoder.

Image width.

Output chroma format.

See also:
XDM_ChromaFormat

Total number of Access Units.

Total number of scans.

Input and output buffer information.

See also:
XDM_AlgBufInfo

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated