Data Fields

IIMGDEC1_Params Struct Reference
[IIMGDEC1 - XDM Image Decoder Interface]

Defines the creation time parameters for all IIMGDEC1 instance objects. More...

#include <iimgdec1.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 maxHeight
XDAS_Int32 maxWidth
XDAS_Int32 maxScans
XDAS_Int32 dataEndianness
XDAS_Int32 forceChromaFormat

Detailed Description

Defines the creation time parameters for all IIMGDEC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Maximum image height.

Maximum image width.

Maximum number of scans.

Endianness of output data.

See also:
XDM_DataFormat

Chroma formats.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
See also:
XDM_ChromaFormat.

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated