Data Structures | Defines | Typedefs

IVIDENC1 - XDM Video Encoder Interface

Data Structures

struct  IVIDENC1_Obj
 This must be the first field of all IVIDENC1 instance objects. More...
struct  IVIDENC1_Params
 Defines the creation time parameters for all IVIDENC1 instance objects. More...
struct  IVIDENC1_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
struct  IVIDENC1_InArgs
 Defines the input arguments for all IVIDENC1 instance process function. More...
struct  IVIDENC1_Status
 Defines instance status parameters. More...
struct  IVIDENC1_OutArgs
 Defines the run time output arguments for all IVIDENC1 instance objects. More...
struct  IVIDENC1_MbData
 Defines the structure that contains macroblock related encoding parameter estimates. More...
struct  IVIDENC1_Fxns
 Defines all of the operations on IVIDENC1 objects. More...

Defines

#define IVIDENC1_EOK   XDM_EOK
#define IVIDENC1_EFAIL   XDM_EFAIL
#define IVIDENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef struct IVIDENC1_Obj IVIDENC1_Obj
 This must be the first field of all IVIDENC1 instance objects.
typedef struct IVIDENC1_ObjIVIDENC1_Handle
 Opaque handle to an IVIDENC1 objects.
typedef struct IVIDENC1_Params IVIDENC1_Params
 Defines the creation time parameters for all IVIDENC1 instance objects.
typedef struct
IVIDENC1_DynamicParams 
IVIDENC1_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls.
typedef struct IVIDENC1_InArgs IVIDENC1_InArgs
 Defines the input arguments for all IVIDENC1 instance process function.
typedef struct IVIDENC1_Status IVIDENC1_Status
 Defines instance status parameters.
typedef struct IVIDENC1_OutArgs IVIDENC1_OutArgs
 Defines the run time output arguments for all IVIDENC1 instance objects.
typedef IALG_Cmd IVIDENC1_Cmd
 Defines the control commands for the IVIDENC1 module.
typedef struct IVIDENC1_MbData IVIDENC1_MbData
 Defines the structure that contains macroblock related encoding parameter estimates.
typedef struct IVIDENC1_Fxns IVIDENC1_Fxns
 Defines all of the operations on IVIDENC1 objects.

Detailed Description

This is the XDM IVIDENC1 Video Encoder Interface.


Define Documentation

#define IVIDENC1_EOK   XDM_EOK

Success.

#define IVIDENC1_EFAIL   XDM_EFAIL

General failure.

#define IVIDENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct IVIDENC1_Obj IVIDENC1_Obj

This must be the first field of all IVIDENC1 instance objects.

typedef struct IVIDENC1_Obj* IVIDENC1_Handle

Opaque handle to an IVIDENC1 objects.

Defines the creation time parameters for all IVIDENC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

This structure defines the algorithm parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDENC1_Fxns::control()

Defines the input arguments for all IVIDENC1 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDENC1_Fxns::process()

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDENC1_Fxns::control()

Defines the run time output arguments for all IVIDENC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDENC1_Fxns::process()

Defines the control commands for the IVIDENC1 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDENC1_Fxns::control()

Defines the structure that contains macroblock related encoding parameter estimates.

Remarks:
An array of IVIDENC1_MbData is provided within the inBufs parameter to IVIDENC1_Fxns::process() when IVIDENC1_DynamicParams::mbDataFlag is set.
See also:
IVIDENC1_DynamicParams::mbDataFlag
IVIDENC1_Fxns::process()
IVIDENC1_Fxns::control()
typedef struct IVIDENC1_Fxns IVIDENC1_Fxns

Defines all of the operations on IVIDENC1 objects.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated