Data Structures | Defines | Typedefs

IVIDENC - XDM Video Encoder Interface

Data Structures

struct  IVIDENC_Obj
 This must be the first field of all IVIDENC instance objects. More...
struct  IVIDENC_Params
 Defines the creation time parameters for all IVIDENC instance objects. More...
struct  IVIDENC_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  IVIDENC_InArgs
 Defines the input arguments for all IVIDENC instance process function. More...
struct  IVIDENC_Status
 Defines instance status parameters (read-only). More...
struct  IVIDENC_OutArgs
 Defines the run time output arguments for all IVIDENC instance objects. More...
struct  IVIDENC_Fxns
 Defines all of the operations on IVIDENC objects. More...

Defines

#define IVIDENC_CID   "ti.xdais.dm.IVIDENC"
#define IVIDENC_ERUNTIME   XDM_ERUNTIME
#define IVIDENC_EOK   XDM_EOK
#define IVIDENC_EFAIL   XDM_EFAIL

Typedefs

typedef struct IVIDENC_Obj IVIDENC_Obj
 This must be the first field of all IVIDENC instance objects.
typedef struct IVIDENC_ObjIVIDENC_Handle
 Opaque handle to an IVIDENC objects.
typedef struct IVIDENC_Params IVIDENC_Params
 Defines the creation time parameters for all IVIDENC instance objects.
typedef struct
IVIDENC_DynamicParams 
IVIDENC_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls.
typedef struct IVIDENC_InArgs IVIDENC_InArgs
 Defines the input arguments for all IVIDENC instance process function.
typedef struct IVIDENC_Status IVIDENC_Status
 Defines instance status parameters (read-only).
typedef struct IVIDENC_OutArgs IVIDENC_OutArgs
 Defines the run time output arguments for all IVIDENC instance objects.
typedef IALG_Cmd IVIDENC_Cmd
 Defines the control commands for the IVIDENC module.
typedef struct IVIDENC_Fxns IVIDENC_Fxns
 Defines all of the operations on IVIDENC objects.

Detailed Description

This is the XDM IVIDENC Video Encoder Interface.

Deprecated:
This XDM video encoder interface has been deprecated, and superceeded by newer IVIDENCx video encoder interfaces.

Define Documentation

#define IVIDENC_CID   "ti.xdais.dm.IVIDENC"

IVIDENC Class ID

#define IVIDENC_ERUNTIME   XDM_ERUNTIME

General runtime failure.

#define IVIDENC_EOK   XDM_EOK

Success.

#define IVIDENC_EFAIL   XDM_EFAIL

General failure.


Typedef Documentation

typedef struct IVIDENC_Obj IVIDENC_Obj

This must be the first field of all IVIDENC instance objects.

typedef struct IVIDENC_Obj* IVIDENC_Handle

Opaque handle to an IVIDENC objects.

Defines the creation time parameters for all IVIDENC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDENC_Fxns::control()

Defines the input arguments for all IVIDENC instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDENC_Fxns::process()

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDENC_Fxns::control()

Defines the run time output arguments for all IVIDENC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDENC_Fxns::process()

Defines the control commands for the IVIDENC module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDENC_Fxns::control()
typedef struct IVIDENC_Fxns IVIDENC_Fxns

Defines all of the operations on IVIDENC objects.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated