Data Structures | Defines | Typedefs

IVIDDEC - XDM Video Decoder Interface

Data Structures

struct  IVIDDEC_Obj
 This must be the first field of all IVIDDEC instance objects. More...
struct  IVIDDEC_Params
 Defines the creation time parameters for all IVIDDEC instance objects. More...
struct  IVIDDEC_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  IVIDDEC_InArgs
 Defines the input arguments for all IVIDDEC instance process function. More...
struct  IVIDDEC_Status
 Defines instance status parameters. More...
struct  IVIDDEC_OutArgs
 Defines the run time output arguments for all IVIDDEC instance objects. More...
struct  IVIDDEC_Fxns
 Defines all of the operations on IVIDDEC objects. More...

Defines

#define IVIDDEC_CID   "ti.xdais.dm.IVIDDEC"
#define IVIDDEC_ERUNTIME   XDM_ERUNTIME
#define IVIDDEC_EOK   XDM_EOK
#define IVIDDEC_EFAIL   XDM_EFAIL

Typedefs

typedef struct IVIDDEC_Obj IVIDDEC_Obj
 This must be the first field of all IVIDDEC instance objects.
typedef struct IVIDDEC_ObjIVIDDEC_Handle
 Opaque handle to an IVIDDEC objects.
typedef struct IVIDDEC_Params IVIDDEC_Params
 Defines the creation time parameters for all IVIDDEC instance objects.
typedef struct
IVIDDEC_DynamicParams 
IVIDDEC_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls.
typedef struct IVIDDEC_InArgs IVIDDEC_InArgs
 Defines the input arguments for all IVIDDEC instance process function.
typedef struct IVIDDEC_Status IVIDDEC_Status
 Defines instance status parameters.
typedef struct IVIDDEC_OutArgs IVIDDEC_OutArgs
 Defines the run time output arguments for all IVIDDEC instance objects.
typedef IALG_Cmd IVIDDEC_Cmd
 Defines the control commands for the IVIDDEC module.
typedef struct IVIDDEC_Fxns IVIDDEC_Fxns
 Defines all of the operations on IVIDDEC objects.

Detailed Description

This is the XDM IVIDDEC Video Decoder Interface.

Deprecated:
This XDM video decoder interface has been deprecated, and superceeded by newer IVIDDECx video decoder interfaces.

Define Documentation

#define IVIDDEC_CID   "ti.xdais.dm.IVIDDEC"

IVIDDEC Class ID

#define IVIDDEC_ERUNTIME   XDM_ERUNTIME

General runtime failure.

#define IVIDDEC_EOK   XDM_EOK

Success.

#define IVIDDEC_EFAIL   XDM_EFAIL

General failure.


Typedef Documentation

typedef struct IVIDDEC_Obj IVIDDEC_Obj

This must be the first field of all IVIDDEC instance objects.

typedef struct IVIDDEC_Obj* IVIDDEC_Handle

Opaque handle to an IVIDDEC objects.

Defines the creation time parameters for all IVIDDEC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.
This structure may be extended by individual codec implementation allowing customization with vendor specific parameters.
The size field must be correctly set by the caller.

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC_Fxns::control()

Defines the input arguments for all IVIDDEC instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC_Fxns::process()

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC_Fxns::control()

Defines the run time output arguments for all IVIDDEC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC_Fxns::process()

Defines the control commands for the IVIDDEC module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDDEC_Fxns::control()
typedef struct IVIDDEC_Fxns IVIDDEC_Fxns

Defines all of the operations on IVIDDEC objects.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated