Data Structures | Defines | Typedefs | Enumerations

ISPHDEC1 - XDM Speech Decoder Interface

Data Structures

struct  ISPHDEC1_Obj
 This must be the first field of all ISPHDEC1 instance objects. More...
struct  ISPHDEC1_Params
 Defines the creation time parameters for all ISPHDEC1 instance objects. More...
struct  ISPHDEC1_DynamicParams
 This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control(). More...
struct  ISPHDEC1_InArgs
 Defines the input arguments for all ISPHDEC1 instance process function. More...
struct  ISPHDEC1_Status
 Defines instance status parameters. More...
struct  ISPHDEC1_OutArgs
 Defines the run time output arguments for all ISPHDEC1 instance objects. More...
struct  ISPHDEC1_Fxns
 Defines all of the operations on ISPHDEC1 objects. More...

Defines

#define ISPHDEC1_EOK   XDM_EOK
#define ISPHDEC1_EFAIL   XDM_EFAIL
#define ISPHDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef struct ISPHDEC1_Obj ISPHDEC1_Obj
 This must be the first field of all ISPHDEC1 instance objects.
typedef struct ISPHDEC1_ObjISPHDEC1_Handle
 Opaque handle to an ISPHDEC1 objects.
typedef struct ISPHDEC1_Params ISPHDEC1_Params
 Defines the creation time parameters for all ISPHDEC1 instance objects.
typedef struct
ISPHDEC1_DynamicParams 
ISPHDEC1_DynamicParams
 This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control().
typedef struct ISPHDEC1_InArgs ISPHDEC1_InArgs
 Defines the input arguments for all ISPHDEC1 instance process function.
typedef struct ISPHDEC1_Status ISPHDEC1_Status
 Defines instance status parameters.
typedef struct ISPHDEC1_OutArgs ISPHDEC1_OutArgs
 Defines the run time output arguments for all ISPHDEC1 instance objects.
typedef IALG_Cmd ISPHDEC1_Cmd
 Defines the control commands for the ISPHDEC1 module.
typedef struct ISPHDEC1_Fxns ISPHDEC1_Fxns
 Defines all of the operations on ISPHDEC1 objects.

Enumerations

enum  ISPHDEC1_FrameType {
  ISPHDEC1_FTYPE_SPEECHGOOD = 0,
  ISPHDEC1_FTYPE_SIDUPDATE = 1,
  ISPHDEC1_FTYPE_NODATA = 2,
  ISPHDEC1_FTYPE_SPEECHLOST = 3,
  ISPHDEC1_FTYPE_DEGRADED = 4,
  ISPHDEC1_FTYPE_BAD = 5,
  ISPHDEC1_FTYPE_SIDFIRST = 6,
  ISPHDEC1_FTYPE_SIDBAD = 7,
  ISPHDEC1_FTYPE_ONSET = 8
}
 

Decoder frame types.

More...

Detailed Description

This is the XDM ISPHDEC1 Speech Decoder Interface.


Define Documentation

#define ISPHDEC1_EOK   XDM_EOK

Success.

#define ISPHDEC1_EFAIL   XDM_EFAIL

General failure.

#define ISPHDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct ISPHDEC1_Obj ISPHDEC1_Obj

This must be the first field of all ISPHDEC1 instance objects.

typedef struct ISPHDEC1_Obj* ISPHDEC1_Handle

Opaque handle to an ISPHDEC1 objects.

Defines the creation time parameters for all ISPHDEC1 instance objects.

Remarks:
Some of the fields in this structure are optional and depend on the class of speech decoder you're creating.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control().

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHDEC1_Fxns::control()

Defines the input arguments for all ISPHDEC1 instance process function.

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHDEC1_Fxns::control()

Defines the run time output arguments for all ISPHDEC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHDEC1_Fxns::process()

Defines the control commands for the ISPHDEC1 module.

Remarks:
This ID can be extended in IMOD interface for additional control commands.
See also:
XDM_CmdId
ISPHDEC1_Fxns::control()
typedef struct ISPHDEC1_Fxns ISPHDEC1_Fxns

Defines all of the operations on ISPHDEC1 objects.


Enumeration Type Documentation

Decoder frame types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
See also:
ISPHDEC1_InArgs.frameType
Enumerator:
ISPHDEC1_FTYPE_SPEECHGOOD 

Regular speech frame received without errors/loss.

ISPHDEC1_FTYPE_SIDUPDATE 

SID update frames.

ISPHDEC1_FTYPE_NODATA 

Untransmitted frame for codecs which support internal DTX.

ISPHDEC1_FTYPE_SPEECHLOST 

Complete loss of speech frame.

ISPHDEC1_FTYPE_DEGRADED 

Speech frame with a correct CRC, some invalid data.

ISPHDEC1_FTYPE_BAD 

Speech frame (likely), but invalid.

ISPHDEC1_FTYPE_SIDFIRST 

The first frame of comfort noise.

ISPHDEC1_FTYPE_SIDBAD 

Corrupt SID update frame.

ISPHDEC1_FTYPE_ONSET 

Frames which precede the first speech frame of a speech burst.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated