Data Structures | Defines | Typedefs

IIMGENC1 - XDM Image Encoder Interface

Data Structures

struct  IIMGENC1_Obj
 This must be the first field of all IIMGENC1 instance objects. More...
struct  IIMGENC1_Params
 Defines the creation time parameters for all IIMGENC1 instance objects. More...
struct  IIMGENC1_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
struct  IIMGENC1_InArgs
 Defines the input arguments for all IIMGENC1 instance process() function. More...
struct  IIMGENC1_Status
 Defines instance status parameters. More...
struct  IIMGENC1_OutArgs
 Defines the run time output arguments for all IIMGENC1 instance objects. More...
struct  IIMGENC1_Fxns
 Defines all of the operations on IIMGENC1 objects. More...

Defines

#define IIMGENC1_EOK   XDM_EOK
#define IIMGENC1_EFAIL   XDM_EFAIL
#define IIMGENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef struct IIMGENC1_Obj IIMGENC1_Obj
 This must be the first field of all IIMGENC1 instance objects.
typedef struct IIMGENC1_ObjIIMGENC1_Handle
 Opaque handle to an IIMGENC1 objects.
typedef struct IIMGENC1_Params IIMGENC1_Params
 Defines the creation time parameters for all IIMGENC1 instance objects.
typedef struct
IIMGENC1_DynamicParams 
IIMGENC1_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls.
typedef struct IIMGENC1_InArgs IIMGENC1_InArgs
 Defines the input arguments for all IIMGENC1 instance process() function.
typedef struct IIMGENC1_Status IIMGENC1_Status
 Defines instance status parameters.
typedef struct IIMGENC1_OutArgs IIMGENC1_OutArgs
 Defines the run time output arguments for all IIMGENC1 instance objects.
typedef IALG_Cmd IIMGENC1_Cmd
 Defines the control commands for the IIMGENC1 module.
typedef struct IIMGENC1_Fxns IIMGENC1_Fxns
 Defines all of the operations on IIMGENC1 objects.

Detailed Description

This is the XDM IIMGENC1 Image Encoder Interface.


Define Documentation

#define IIMGENC1_EOK   XDM_EOK

Success.

#define IIMGENC1_EFAIL   XDM_EFAIL

General failure.

#define IIMGENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct IIMGENC1_Obj IIMGENC1_Obj

This must be the first field of all IIMGENC1 instance objects.

typedef struct IIMGENC1_Obj* IIMGENC1_Handle

Opaque handle to an IIMGENC1 objects.

Defines the creation time parameters for all IIMGENC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

This structure defines the algorithm parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC1_Fxns::control()

Defines the input arguments for all IIMGENC1 instance process() function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC1_Fxns::process()

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC1_Fxns::control()

Defines the run time output arguments for all IIMGENC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC1_Fxns::process()

Defines the control commands for the IIMGENC1 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IIMGENC1_Fxns::control()
typedef struct IIMGENC1_Fxns IIMGENC1_Fxns

Defines all of the operations on IIMGENC1 objects.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated