Data Structures | Defines | Typedefs

IAUDENC1 - Audio Encoder Interface

Data Structures

struct  IAUDENC1_Obj
 This must be the first field of all IAUDENC1 instance objects. More...
struct  IAUDENC1_Params
 Defines the creation time parameters for all IAUDENC1 instance objects. More...
struct  IAUDENC1_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
struct  IAUDENC1_InArgs
 Defines the input arguments for all IAUDENC1 instance process function. More...
struct  IAUDENC1_Status
 Defines instance status parameters (read-only). More...
struct  IAUDENC1_OutArgs
 Defines the run time output arguments for all IAUDENC1 instance objects. More...
struct  IAUDENC1_Fxns
 Defines all of the operations on IAUDENC1 objects. More...

Defines

#define IAUDENC1_EOK   XDM_EOK
#define IAUDENC1_EFAIL   XDM_EFAIL
#define IAUDENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef struct IAUDENC1_Obj IAUDENC1_Obj
 This must be the first field of all IAUDENC1 instance objects.
typedef struct IAUDENC1_ObjIAUDENC1_Handle
 Opaque handle to an IAUDENC1 objects.
typedef struct IAUDENC1_Params IAUDENC1_Params
 Defines the creation time parameters for all IAUDENC1 instance objects.
typedef struct
IAUDENC1_DynamicParams 
IAUDENC1_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls.
typedef struct IAUDENC1_InArgs IAUDENC1_InArgs
 Defines the input arguments for all IAUDENC1 instance process function.
typedef struct IAUDENC1_Status IAUDENC1_Status
 Defines instance status parameters (read-only).
typedef struct IAUDENC1_OutArgs IAUDENC1_OutArgs
 Defines the run time output arguments for all IAUDENC1 instance objects.
typedef IALG_Cmd IAUDENC1_Cmd
 Defines the control commands for the IAUDENC1 module.
typedef struct IAUDENC1_Fxns IAUDENC1_Fxns
 Defines all of the operations on IAUDENC1 objects.

Detailed Description

This is the XDM IAUDENC1 Audio Encoder Interface.


Define Documentation

#define IAUDENC1_EOK   XDM_EOK

Success.

#define IAUDENC1_EFAIL   XDM_EFAIL

General failure.

#define IAUDENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct IAUDENC1_Obj IAUDENC1_Obj

This must be the first field of all IAUDENC1 instance objects.

typedef struct IAUDENC1_Obj* IAUDENC1_Handle

Opaque handle to an IAUDENC1 objects.

Defines the creation time parameters for all IAUDENC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

This structure defines the algorithm parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IAUDENC1_Fxns::control()

Defines the input arguments for all IAUDENC1 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IAUDENC1_Fxns::process()

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IAUDENC1_Fxns::control()

Defines the run time output arguments for all IAUDENC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IAUDENC1_Fxns::process()

Defines the control commands for the IAUDENC1 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IAUDENC1_Fxns::control()
typedef struct IAUDENC1_Fxns IAUDENC1_Fxns

Defines all of the operations on IAUDENC1 objects.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated