Defines the structure that contains macroblock related encoding parameter estimates. More...
#include <ividenc1.h>
Data Fields | |
XDAS_Int32 | mbMode |
XDAS_Int32 | QP |
XDAS_Int32 | mvFwdXY |
XDAS_Int32 | mvBwdXY |
Defines the structure that contains macroblock related encoding parameter estimates.
inBufs
parameter to IVIDENC1_Fxns::process() when IVIDENC1_DynamicParams::mbDataFlag is set.MB encoding mode
QP estimate.
Forward Motion vector estimate.
mvFwdXY = ((MVx & 0x0000FFFF) << 16) | (MVy & 0x0000FFFF);
Backward motion vector estimate.