Data Structures | Defines | Typedefs

IIMGENC - XDM Image Encoder Interface

Data Structures

struct  IIMGENC_Obj
 This must be the first field of all IIMGENC instance objects. More...
struct  IIMGENC_Params
 Defines the creation time parameters for all IIMGENC instance objects. More...
struct  IIMGENC_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
struct  IIMGENC_InArgs
 Defines the input arguments for all IIMGENC instance process() function. More...
struct  IIMGENC_Status
 Defines instance status parameters (read-only). More...
struct  IIMGENC_OutArgs
 Defines the run time output arguments for all IIMGENC instance objects. More...
struct  IIMGENC_Fxns
 Defines all of the operations on IIMGENC objects. More...

Defines

#define IIMGENC_CID   "ti.xdais.dm.IIMGENC"
#define IIMGENC_ERUNTIME   XDM_ERUNTIME
#define IIMGENC_EOK   XDM_EOK
#define IIMGENC_EFAIL   XDM_EFAIL

Typedefs

typedef struct IIMGENC_Obj IIMGENC_Obj
 This must be the first field of all IIMGENC instance objects.
typedef struct IIMGENC_ObjIIMGENC_Handle
 Opaque handle to an IIMGENC objects.
typedef struct IIMGENC_Params IIMGENC_Params
 Defines the creation time parameters for all IIMGENC instance objects.
typedef struct
IIMGENC_DynamicParams 
IIMGENC_DynamicParams
 This structure defines the algorithm parameters that can be modified after creation via control() calls.
typedef struct IIMGENC_InArgs IIMGENC_InArgs
 Defines the input arguments for all IIMGENC instance process() function.
typedef struct IIMGENC_Status IIMGENC_Status
 Defines instance status parameters (read-only).
typedef struct IIMGENC_OutArgs IIMGENC_OutArgs
 Defines the run time output arguments for all IIMGENC instance objects.
typedef IALG_Cmd IIMGENC_Cmd
 Defines the control commands for the IIMGENC module.
typedef struct IIMGENC_Fxns IIMGENC_Fxns
 Defines all of the operations on IIMGENC objects.

Detailed Description

This is the XDM IIMGENC Image Encoder Interface.

Deprecated:
This XDM image encoder interface has been deprecated, and superceeded by newer IIMGENCx image encoder interfaces.

Define Documentation

#define IIMGENC_CID   "ti.xdais.dm.IIMGENC"

IIMGENC Class ID

#define IIMGENC_ERUNTIME   XDM_ERUNTIME

General runtime failure.

#define IIMGENC_EOK   XDM_EOK

Success.

#define IIMGENC_EFAIL   XDM_EFAIL

General failure.


Typedef Documentation

typedef struct IIMGENC_Obj IIMGENC_Obj

This must be the first field of all IIMGENC instance objects.

typedef struct IIMGENC_Obj* IIMGENC_Handle

Opaque handle to an IIMGENC objects.

Defines the creation time parameters for all IIMGENC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

This structure defines the algorithm parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC_Fxns::control()

Defines the input arguments for all IIMGENC instance process() function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC_Fxns::process()

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC_Fxns::control()

Defines the run time output arguments for all IIMGENC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IIMGENC_Fxns::process()

Defines the control commands for the IIMGENC module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IIMGENC_Fxns::control()
typedef struct IIMGENC_Fxns IIMGENC_Fxns

Defines all of the operations on IIMGENC objects.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated