IVIDENC_Params Struct Reference
[IVIDENC - XDM Video Encoder Interface]

Defines the creation time parameters for all IVIDENC instance objects. More...

#include <ividenc.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 encodingPreset
XDAS_Int32 rateControlPreset
XDAS_Int32 maxHeight
XDAS_Int32 maxWidth
XDAS_Int32 maxFrameRate
XDAS_Int32 maxBitRate
XDAS_Int32 dataEndianness
XDAS_Int32 maxInterFrameInterval
XDAS_Int32 inputChromaFormat
XDAS_Int32 inputContentType

Detailed Description

Defines the creation time parameters for all IVIDENC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Encoding preset.

Video rate control presets.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE

See also:
IVIDEO_RateControlPreset

Maximum height.

Maximum width.

Maximum frame rate * 1000.

Maximum bit rate, bits per second.

Endianness of output data.

See also:
XDM_DataFormat

I to P frame distance. e.g. = 1 if no B frames, 2 to insert one B frame.

Chroma format for the input buffer.

See also:
XDM_ChromaFormat

Video content type of the buffer being encoded.

See also:
IVIDEO_ContentType

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated