IVIDDEC_DynamicParams Struct Reference
[IVIDDEC - XDM Video Decoder Interface]

This structure defines the codec parameters that can be modified after creation via control() calls. More...

#include <ividdec.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 decodeHeader
XDAS_Int32 displayWidth
XDAS_Int32 frameSkipMode

Detailed Description

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller.
See also:
IVIDDEC_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Number of access units to decode.

See also:
XDM_DecMode

Pitch. If set to zero, use the decoded image width. Else, use given display width in pixels.

Frame skip mode.

See also:
IVIDEO_FrameSkip

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated