Defines instance status parameters. More...
#include <ividdec3.h>
Defines instance status parameters.
size
parameter. size
field must be correctly set by the caller.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Extended error information.
Buffer descriptor for data passing.
data.buf
to NULL.The maximum number of buffers that will be required by the codec.
The maximum number of display buffers that can be returned via IVIDDEC3_OutArgs.displayBufs.
Output height in pixels.
Output width in pixels.
Average frame rate in fps * 1000. For example, if average frame rate is 30 frames per second, this field should be 30000.
Average bit rate, in bits per second.
Video content types.
Sample aspect ratio height.
Sample aspect ratio width.
Full 8 bit, CCIR 601
Output chroma format.
Video decoding mode of operation.
Frame Order
Input data mode.
Output data mode.
Input and output buffer information.
Number of input slices/rows.
Number of output slices/rows.
outputDataMode
, like number of slices/rows/blocks etc.Configuration ID of given codec.
XDAS_Int32 IVIDDEC3_Status::metadataType[IVIDEO_MAX_NUM_METADATA_PLANES] |
Type of each metadata plane.
Current values of the decoder's dynamic parameters.